A man in a lab coat looking at a digital twin of an aircraft engine

5 Requirements Your Network Emulator Tool Must Satisfy

As communication networks become ubiquitous, there is continuous innovation both in the technologies they employ and the services they are expected to provide, creating new challenges for equipment manufacturers, service providers, network planners, and operators. Network emulation can assist in addressing many of these challenges, including:

For a network emulation tool to add value and provide a high return on investment for users — network operators, planners, designers, testers or analysts — it must satisfy the following requirements:

  1. Accuracy

Network emulations must be able to accurately reproduce the behavior of the corresponding network as it operates in the field. To achieve this, the simulator must model the network devices, end-to-end protocols, traffic, and the operational environment accurately and at the appropriate fidelity. Emulators that use abstractions to reduce model execution time (e.g., by ignoring terrain effects or buffer size or bursty traffic patterns) will fail to capture the network dynamics which significantly affect network performance and lead to potential issues like congestion, voice quality degradations, or failures.

  1. Speed and Scalability

Multiple emulation runs are typically needed to obtain statistically valid and meaningful results, so fast execution speed — without sacrificing accuracy — is essential. As network size increases, the emulation time often increases non-linearly with size and traffic volume. As network dynamics of large networks are very different from smaller networks, extrapolation of results obtained by simulating small networks to larger networks is difficult. Therefore, for the simulation tool to be useful, it must be able to run ‘at-scale' models faster than real-time without sacrificing accuracy.

  1. Ease of Creating Emulation Models

Developing high-fidelity models of network devices and protocols from scratch is time consuming and also requires detailed networking knowledge together with programming expertise. Thus, to provide a high return on investment, network simulators must facilitate rapid model creation.

  1. Ease of Network Visualization and Performance Analysis

The results from a network emulation are used for network analysis and to provide insight into network operations. To facilitate this, the emulation tool should have the following features:

  1. Ability to Interface with Live Applications

The network emulation must be able to interface with live network components and real applications. This in turn requires that the emulation run in hard real-time. In other words, the application will interact with the simulated network exactly as it interacts with the corresponding live network. This enables an analyst to directly assess the application's performance under different operating conditions, such as different terrains or mobility paths, simply by modifying appropriate parameters of the network model. Similarly, such emulations can be used to investigate potential interference among applications under different operating conditions like varying levels of traffic intensity. This provides a low-cost and high return on investment alternative to performing such assessments using physical testbeds.

Keysight EXata network digital twin solution can run accurate, at-scale network emulations faster than real-time, support an extensive library of network models, and provide a suite of tools for scenario creation and network visualization and analysis. Find out how network emulation can give you a preemptive defense against the worst cyberattacks in our blog Zero-Day Attacks and What Organizations Can Do To Prevent Them.

limit
3