The power of seamless CI/CD integrations with DAI 6.2.1
In the latest release of Eggplant Digital Automation Intelligence (DAI), we’ve enhanced our integrations with GitHub, Jenkins, and Azure DevOps. DAI 6.2.1 allows users to export results to test case management platforms helping to increase visibility and identify issues faster.
What’s a CI/CD pipeline?
A Continuous Integration/Continuous Delivery pipeline (CI/CD pipeline) automates software delivery processes. It’s a highly efficient method consisting of building code, running tests (CI), and deploying new releases or applications faster.
What does CI/CD mean?
Continuous Integration (CI) is a software development practice in which all developers merge code changes in a central repository multiple times a day. Continuous Delivery (CD) is the practice of automating the entire software release process.
Continuous Delivery includes infrastructure provisioning and deployment, which may be manual and consist of multiple stages. What’s important is that all these processes are fully automated, with each run fully logged and visible to the entire team.
Benefits of CI/CD integrations
Embed Eggplant in your ecosystem to perform fully automated, deployment and end-to-end testing of your applications.
Download Eggplant Runner straight from your CI/CD platform’s marketplace.
Benefits of powerful CI/CD integrations with DAI 6.2.1
- Accelerate deployments to meet the demands of faster release cycles.
- Reduce risk and remain competitive by deploying quality code multiple times a day.
- Enhance collaboration with better visibility across multiple teams.
- Reduce manual effort with auto triggers and actions across the software development lifecycle (SDLC).
- Better troubleshooting capabilities with access to logs from each stage from the development process.
Easily export test results
DAI 6.2.1 allows all CI/CD integrations to return results of tests triggered as part of the build pipeline.
DAI 6.2.1 can also help users improve traceability of previous tests by allowing them to see all tests in DAI or your chosen build platform. Accelerate continuous integration and continuous delivery by integrating Eggplant into your end-to-end application lifecycle management tooling.
See DAI 6.2.1 for yourself
For existing DAI users, you can upgrade to 6.2.1 by following the instructions in our documentation portal. Users of the browser-based version of DAI will have immediate access to the new features.
If you have any questions or want to connect with one of our test automation experts, please get in touch. If you aren’t yet an Eggplant customer, you can easily sign up for a free trial of DAI here.
Useful links
To download Eggplant API plugins on CI systems, please use the links below: