From Manual Missions to Machine Intelligence: Aerospace and Defense’s Shift to AI-Augmented Software Quality
Long before DevOps and continuous testing became part of the defense vocabulary, software testers in aerospace and defense (A&D) worked with clipboards, manual checklists, and meticulous patience. They verified flight control systems, command-and-control applications, and radar interfaces step by step. Often inside sealed labs where even a misplaced USB drive required paperwork.
Back then, testing cycles were slow, repetitive, and nerve-wracking. When automation tools like Selenium, QTP, or custom Python scripts began to appear, many QA teams saw hope. But those frameworks, built for open web applications, faltered in classified environments.
As soon as a cockpit interface changed or a label moved by a few pixels, tests broke. In air-gapped labs, fixing a single script could take hours of coordination and clearance. For teams working under contracts tied to DO-178C, MIL-STD-882E, or NIST RMF, every broken test wasn’t just an inconvenience, it meant schedule slips, documentation delays, and potential financial penalties.
The Reality of Testing in Classified Environments
A&D testers operate under conditions that few commercial QA teams could imagine. Most spend close to half their time maintaining fragile automation suites or waiting for access to restricted systems. When a test fails in a secure lab, remote debugging isn’t an option; it often means lost time, rescheduled ranges, and thousands of dollars in sunk costs.
Each test must be auditable and traceable to its original requirement in systems like DOORS or Jama. Certification isn’t just about proving functionality; it’s about providing exhaustive evidence that every possible scenario has been considered, validated, and logged.
In such conditions, even small inefficiencies scale into major setbacks. A single failed regression run can delay a release by weeks, jeopardizing contract milestones and, in extreme cases, mission readiness.
Why Traditional Automation Falls Short
Many open-source and commercial test frameworks were designed for internet-connected enterprise software, not for air-gapped, high-security defense systems. Their limitations are well known:
- They require code or DOM access, which is forbidden on classified systems.
- They rely on network connectivity or cloud integrations, disallowed by DoD cybersecurity policy.
- They fail when UI elements or graphical displays change, causing brittle automation.
- They can’t span hardware, embedded systems, and enterprise applications in one test flow.
Even the best-intentioned QA teams found themselves stuck, unable to modernize because their tools couldn’t cross the boundaries imposed by security and compliance.
The Human Cost: Cognitive Fatigue and Fear of Missed Defects
Testing in defense is as much a psychological challenge as a technical one. QA professionals live with the constant pressure that a missed defect could cost lives, delay deployment, or compromise national security.
Psychologists refer to this as sustained vigilance fatigue, the mental strain of prolonged attention. For testers reviewing thousands of data points or displays under stress, that fatigue is real.
Early automation didn’t help much. Its fragility created automation anxiety - the fear that tests would fail not because of defects, but because the framework couldn’t keep up. Many teams continued to re-run automated results manually “just to be sure,” defeating the purpose of automation altogether.
Confidence returned only when automation became trustworthy, when testers could watch a tool interact with systems visually, capture evidence automatically, and produce compliance-ready results accepted by auditors.
The Turning Point: Non-Invasive, AI-Driven Testing
The emergence of non-invasive, AI-driven automation marked a turning point for the defense sector. Unlike agent-based solutions, these modern platforms don’t install software on mission systems or access source code. Instead, they connect through secure channels, such as VNC, RDP, or Citrix, to observe and control systems exactly as a human operator would.
This approach preserves both security and fidelity. By relying on computer vision and optical character recognition (OCR), non-invasive automation validates the interface itself, verifying that what appears on the screen is what the operator expects to see.
Adding AI elevates this further. Intelligent algorithms can:
- Autonomously generate test cases from requirements or models.
- Adapt to interface changes without script maintenance.
- Prioritize high-risk areas based on defect history or operational context.
- Continuously learn from past results to improve coverage.
For the first time, A&D QA teams can test dynamically, even in restricted networks, without compromising security or accuracy.
From Siloed Testing to System-of-Systems Validation
Historically, A&D testing occurred in silos: avionics teams validated cockpit software, logistics teams tested ERP workflows, and command teams verified C2 applications. Integration happened late, and that’s where most mission-critical defects were found - at the interfaces.
AI-augmented, model-based testing now makes end-to-end validation possible. By creating a digital twin of the system under test, teams can simulate entire operational chains, from pilot input to avionics processing to ground-station data logging.
These models provide coverage visibility across domains that were once disconnected. More importantly, they offer a common language for QA, development, and compliance teams.
The Rise of Continuous Assurance and cATO
Modern DoD directives have made automated testing not just a best practice, but a baseline expectation. DoDI 5000.87 explicitly mandates automated testing “as much as practicable” throughout the software lifecycle.
The next evolution, Continuous Authority to Operate (cATO), pushes compliance into real-time. Instead of months of manual evidence collection, programs can now generate machine-readable OSCAL artifacts automatically from each test run.
That evidence feeds directly into risk dashboards, providing ongoing assurance for auditors and leadership. The result is fewer certification delays and faster, safer deployment cycles.
Lessons from the Field: When Automation Proved Its Worth
One U.S. Army program provides a powerful example. Its software engineering team once ran a 10-hour manual test every three days to validate a tactical communication terminal. By implementing AI-driven, non-invasive automation, the same team began running 24-hour test cycles every day, tripling coverage while freeing engineers to focus on analysis instead of repetition.
The program also exported auto-generated OSCAL evidence into its RMF dashboard, reducing compliance paperwork from three weeks to less than 48 hours. The automation didn’t just make testing faster. It made the process safer, more transparent, and easier to defend under audit.
The Human Shift: From Test Execution to Risk Intelligence
The cultural transformation is just as important as the technical one. Modern QA teams are no longer measured by how many manual test cases they can execute, but by how effectively they manage risk and communicate assurance.
Automation doesn’t eliminate testers; it elevates them. By removing repetitive work, it lets them focus on critical decision-making, human strengths that automation can’t replicate.
This shift also improves morale. With fewer tedious cycles and more meaningful oversight, testers report higher engagement, stronger collaboration, and greater confidence in release decisions.
Keysight Eggplant: Built for the Realities of Defense Testing
While many testing frameworks crumble under the weight of classified constraints, Keysight Eggplant was designed for them.
- Non-invasive architecture: Tests systems visually via computer vision without accessing code.
- AI-driven test design: Keysight Generator transforms DOORS requirements into traceable test assets on-premise, with no cloud dependency.
- Iron Bank accreditation: Certified for use in DoD networks, ensuring compliance with the highest security standards.
- Cross-platform coverage: Supports everything from embedded flight systems to enterprise logistics dashboards, unifying A&D workflows under one framework.
- Audit-ready reporting: Produces traceable, machine-readable compliance data for Continuous ATO environments.
These capabilities allow QA teams to move from reactive testing to proactive assurance — achieving faster releases, higher reliability, and complete audit visibility across secure systems.
The Future of Aerospace and Defense QA
The next generation of defense testers will inherit tools that continuously test, learn, and adapt, but they’ll still rely on the principles forged by today’s experts: precision, discipline, and trust.
Automation is no longer a luxury; it’s a mission enabler. And as A&D organizations push for DevSecOps maturity, the integration of AI-augmented, non-invasive testing will determine who delivers software at the speed of relevance, without ever compromising safety or security.
Keysight Eggplant is helping make that future real: enabling defense programs to test what was once untestable, maintain continuous assurance, and achieve true mission readiness.
Visit our dedicated A&D software testing page for more information.