What is The Next Generation in RF Circuit Simulation and Optimization?

Find out how Keysight RF Circuit Simulation Pro facilitates better RFIC designs and shortens the time-to-market using state-of-the-art RF circuit simulations.

Key takeaways:

Throughout a modern RFIC design and fabrication process, engineers run many types of simulations to verify and validate their decisions, including:

In this blog, we will discuss how Keysight RF Circuit Simulation Professional revamps RF circuit simulation and optimization. Discover how to achieve efficient, accurate designs for even the most complex RF, microwave, and millimeter-wave RFICs and RF 3D heterogeneous integrated (3DHI) modules for 5G/6G, wireless, aerospace, defense, and radar applications.

What is RF circuit simulation in RFIC design?

Figure 1. RFIC design has to balance multiple objectives pulling in different directions

Compared to digital ICs, RFICs are far more sensitive to noise, crosstalk, and parasitics due to high frequency and precision requirements. RFIC specifications impose far more stringent criteria on speed, power, gain, linearity, precision, power consumption, noise, costs, and radiated emissions.

While meeting customer demand for higher speeds, higher frequency bands, more features, and better performance, designers must delicately balance these often conflicting criteria.

The decisions and assumptions related to such balancing start from the schematic capture stage, the first step after the specifications and architectural decisions are made. Identifying all design problems and optimizing all tradeoffs at this early stage is far quicker and cheaper than doing it later. This is why "shift left" has become so important in the semiconductor industry.

By running RF circuit simulations directly against the schematics, designers can quickly explore different choices and assumptions and easily modify designs to achieve optimal tradeoffs. Designers can iteratively:

Figure 2. Types of RF circuit simulations

Some common RF circuit simulations are listed below:

Why is RF circuit simulation important?

Simulations add significant business, productivity, and technical value throughout the development cycle.

Let's see some of the key business and productivity benefits:

There are significant technical benefits as well:

What improvements are needed in next-generation circuit simulation software?

Existing simulation engines can do with some improvements in features and usability. We outline some of them below:

How can innovations in RF circuit optimization reduce simulation time?

We said RFIC designs must balance many stringent and conflicting criteria. Simulators help with that by using optimizers. Optimizers are algorithms that automatically explore the vast design space of a schematic's modifiable parameters, ensuring that all criteria are satisfied optimally.

However, current optimizers have some drawbacks:

These drawbacks are overcome by modern circuit optimization implementations.

First, new algorithms like particleswarmoptimization can handle challenging designs with large-scale variable counts and converge on multiple performance goals with up to 30x speed-up over traditional techniques. These algorithms also avoid local minima traps.

Second, multi-dimensional sweeps and sequences can be saved as workflows to ensure that all required performance specifications are consistently analyzed without requiring repeated configuration.

Third, real-time visualization of the optimization enables teams to quickly determine if an algorithm is effective or needs modification, thereby avoiding wasted simulation time.

Finally, these algorithms support headless operation for batch simulations and deployment on high-performance computing (HPC) machines, resulting in significant speed-ups.

How does Keysight RF Circuit Pro solve your RFIC design challenges?

Figure 3. Keysight RF Circuit Pro

KeysightRF Circuit Pro revamps RF circuit simulation with several technical, performance, and usability improvements.

Integrated workflows

A unified, workflow-baseduser interface efficiently orchestrates simulation and optimization tasks. Setups are saved and reusable across design teams and EDA platforms, facilitating quick and repetitive analysis without the need for repeated configuration.

RF Circuit Pro works identically and integrates natively with all the industry-leading EDA platforms, enabling collaboration and reuse across diverse design teams and toolchains.

Multi-domain simulations can be configured with multi-dimensional sweeps, sequenced, and saved as workflows to ensure that all required performance specifications are consistently analyzed.

Multi-domain simulation algorithms

Figure 4. RF Circuit Pro simulation, optimization, and visualization are consistent across Keysight ADS and other EDA platforms

RF Circuit Pro includes a comprehensive suite of simulation algorithms like frequency, time, envelope, linear, nonlinear, stability, electro-thermal, system, and measurement. Together, they assist in multi-objective optimization of efficiency, EVM, adjacent channel leakage ratio, stability, gain, power supply output, 5G/6G compliance, and more.

Modern optimization algorithms, such as particle swarm and simulated annealing, achieve significant algorithmic speed-ups (of up to 30x) and avoid local minima traps, even for large-scale, multi-objective designs.

Figure 5. Stability margin analysis estimates the amount of instability risk

Advanced techniques, like Winslow probes and stability margin computations, can detect and quantify the stability of a circuit, helping designers avoid difficult-to-debug issues like oscillations.

Separation of analysis and tasks

RF Circuit Pro separates simulation analyses (like S-parameters and envelope) and tasks (like sweeps or optimization) for more efficient parallelization and significant speed-ups.

Parallel computing acceleration

RF Circuit Pro exploits parallel computing resources like local machines or HPC clusters for substantial speed-up (up to 16x) in both simulation and optimization.

Python automation and AI integration

Figure 6. Custom Python optimizer for Nexus

RF Circuit Pro supports deep programmatic control and workflow automation by exposing comprehensive Python application programming interfaces (APIs).

RF Circuit Pro also seamlessly supports the integration of artificial intelligence (AI) and machine learning (ML) models into the simulation and optimization workflow. Designers can utilize neural networks, large language models (LLMs), copilots, and AI agents to enhance productivity and intelligent design.

3D Heterogeneous Integration

RF Circuit Pro supports the simulation of 3DHI aspects, enabling the combination of RFICs, advanced packaging techniques, and off-chip integration with printed circuit boards.

The common Open Access (OA) database enables RFICs designed in Virtuoso or Custom Compiler to be optimized together with off-chip packaging or in 3DHI modules using Nexus.

How does Python integration enable AI-assisted RF designs?

Nexus APIs support the integration of AI and ML algorithms for AI-assisted designs. Designers can integrate specialized ML models like neural networks, LLMs, or AI agents in their simulation and optimization workflows.

External Python-based optimization algorithms (like Pymoo functions) or custom commercial algorithms can be invoked to supplement the already powerful native optimizers.

Functionalizing physical designs via APIs enables massive simulation data collection to pretrain surrogate AI models. These models can then derive full sets of simulation data from extremely sparse data, thus reducing the number of required data points by a factor of 1,500 as well as the time required for the design process.

Get deep design insights with Keysight RF Circuit Pro for RF circuit simulations

In this blog, we demonstrated how simulations can help designers understand and predict the behavior of RF circuit designs at the schematic stage.

Keysight RF Circuit Pro enables such deep understanding through efficient workflows and optimization algorithms.

Learn More

Introduction to RF Circuit Professional Video

RF Circuit Simulation with RF Circuit Pro Product page

RF Circuit Simulation with RF Circuit Pro Webinar

RF Circuit Simulation with RF Circuit Pro Brochure

Free ADS Software trial

Contact us for insights on how to use RF Circuit Pro for your RFIC designs.