A person looking at a computer screen AI-generated content may be incorrect.

Designing Tomorrow’s Quantum Computers with Today’s EDA Tools

Understand the challenges faced by designers of superconducting quantum chips, and explore the pioneering EDA solutions to overcome them.

Key takeaways:

During this International Year ofQuantum Science and Technology, we at Keysight have worked diligently to support quantum engineers in staying at the forefront of the field. In this blog, learn the basics of designing quantum chips, current design trends, challenges, and cutting-edge quantum EDA solutions from Keysight.

Apart from artificial intelligence, quantum technology is the other field driving advances in chip designs. Engineers in this nascent field can get overwhelmed by the advances happening at every level—in fundamental physics, low-level building blocks, and higher-level workflows.

How do quantum chips work?

A quantum chip consists of several qubits (or quantum bits), the fundamental building blocks of quantum computing, analogous to classical transistors.

A quantum processor with N qubits can represent a superposition of 2^N states. Quantum algorithms map their problem spaces to these states, carefully sequence quantum gates to orchestrate entanglement between the N qubits, and create interference such that amplitudes of only desired solutions are amplified.

The ability of quantum computers to represent exponentially large state spaces is key. This quantum advantage is essential for computationally expensive problems that take supercomputers months to solve and intractable problems beyond classical and even high-performance computers. Such issues with commercial uses include:

A white background with text on it AI-generated content may be incorrect.

Figure 1. Qubit technologies

Currently, quantum research teams and startups are exploring multiple approaches to implement qubits. Natural objects or physical systems like trapped ions, quantum dots, diamond vacancies, photonics, cold atoms, or annealing are used to store quantum information.

Figure 2. Josephson junction and transmon qubit

A popular alternative to these natural objects is the use of various superconducting qubits, which employ Josephson junctions. Due to their larger sizes, they're easier to work with compared to natural qubits.

A Josephson junction is a simple circuit created using lithography, like classical semiconductors. It consists of two superconductor layers separated by a thin insulator layer through which electrons can tunnel. When it's cooled to near absolute zero, the entire junction acts like a single object with quantum mechanical behaviors, even though it's macroscopic with millions of atoms.

What are the components of a superconducting qubit quantum system?

Figure 3. Superconducting quantum machine

A typical superconducting quantum machine consists of the following devices:

What are some key aspects when designing superconducting qubits?

Let's look at some of the key aspects of superconducting qubit designs.

Types of qubits

A diagram of a diagram AI-generated content may be incorrect.

Figure 4. Types of qubits

Selecting a suitable Josephson junction qubit is essential. Based on where they store quantum information, there are charge, flux, and phase qubits. They differ in noise sensitivity, anharmonicities, resonance frequency bands, and other properties.

Additionally, qubits can either be planar or three-dimensional. Planar qubits are currently easier to manufacture but more susceptible to noise and decoherence.

Scaling

A computer screen shot of a grid AI-generated content may be incorrect.

Figure 5. Multi-layer qubit design

Two-dimensional layouts are easier to design and simulate but restrict scalability. The layer designs must be three-dimensional to scale up the number of qubits. But that often complicates electromagnetic (EM) interference and cross-talk.

Control and readout

Critical design goals are reliably manipulating qubits using microwave pulses without introducing noise and amplifying qubit states with high fidelity.

Error correction

Robust error correction is critical since quantum chips operate near the noise floor. This is the biggest bottleneck restricting quantum chips to a few hundred qubits.

Grounding Challenges

Engineers must use air bridges and bond wires to prevent unexpected modes of propagation that can cause unwanted interference.

Cryogenic environment

The cryogenic refrigerator maintains Ultra-Low temperatures critical for superconductivity, coherence, and low thermal noise. Temperatures must be stable and maintain reliably.

However, current control and readout systems operate at room temperature outside the refrigerator. The large number of cables connecting them to the qubits complicates cryogenic temperature control, latency, signal integrity, noise, and scalability. So, a key goal is to move the control systems closer to the qubits and operate them at cryogenic temperatures.

What are the quantum parameters of a superconducting chip?

Apart from the above design aspects, the quantum parameters of a chip are critical properties that must be engineered carefully for design optimization. They include:

How do we extract quantum parameters?

There are different ways to extract quantum parameters with computational and accuracy trade-offs:

What are the key concerns when designing quantum amplifiers?

Figure 6. Quantum amplifier layout

Some key concerns of quantum amplifier designs include:

What are the challenges in modeling superconducting qubit devices?

Quantum computing is a new technology that's just starting and has many decades to mature. Several challenges exist both in the technologies themselves and in the design workflows:

How does Keysight EDA streamline superconducting quantum chip design?

Diagram of a diagram of a device modeling AI-generated content may be incorrect.

Figure 7. Quantum chip design cycle

Keysight's quantumelectronics design automation (EDA) solutions address all the above technology and process challenges through seamless end-to-end workflows to streamline quantum chip and system designs.

The quantum design tools bundled with Keysight Advanced Design System (ADS) provide cutting-edge capabilities to help manufacturers accelerate and scale up their research and design efforts.

Quantum circuits and layouts

Figure 8. Quantum chip layouts in ADS

ADS Layout includes built-in support for quantum layouts with features like:

QuantumPro

A screenshot of a computer AI-generated content may be incorrect.

Figure 9. QuantumPro

QuantumPro offers an integrated electromagnetic (EM) and parameter extraction environment to speed up superconducting qubit designs and create robust quantum computers. It supports:

EMPro

Keysight EM Design (EMPro) accelerates the design of3D superconducting qubits by enabling:

Quantum Circuit Simulation (Quantum Ckt Sim)

A screenshot of a computer AI-generated content may be incorrect.

Figure 11. Quantum Ckt Sim

Quantum Circuit Sim accurately simulates large, highly nonlinear quantum circuits to gain insights into complex amplifiers like JTWPAs.

A diagram of a snake and snail AI-generated content may be incorrect.

Figure 12. Different types of supported complex quantum devices

Quantum Circuit Sim supports:

Scripting and automation

All the above tools publish application programming interfaces and support Python scripts, enabling your quantum computer scientists, physicists, design engineers, and test engineers to automate, customize, and verify all research and design workflows.

From quantum hype to breakthroughs with Keysight EDA

This blog provides a high-level overview of quantum chip design and the current challenges in the field. You saw how Keysight addresses these challenges with innovative, end-to-end EDA workflows.

Contact us for insights, demos, and solutions for your quantum chip design challenges.

Learn more

Quantum Electronics Design Software | Keysight

Bootcamp: Superconducting Quantum Design Challenges