A person typing on a computer AI-generated content may be incorrect.

What is the WirelessPro 3GPP AI Simulation Platform?

Discover how the WirelessPro 3GPP AI simulation platform accelerates time-to-insight, aligning with the rapid 5G/6G development roadmaps.

Key takeaways:

The complex 5G/6G standards being released will put enormous time-to-market pressures on telecom engineers and researchers for the next five years. However, no engineer would want to compromise on design correctness and capabilities due to a lack of time.

Keysight WirelessPro resolves this tension by providing competent research, prototyping, and simulation tools that accelerate comprehensive experimentation on 5G, 5G-Advanced, and 6G designs.

This blog post introduces the Keysight WirelessPro 3GPP AI simulation platform to communication system engineers and researchers responsible for designing, simulating, and validating 5G/6G systems in telecom companies, research institutions, chipset manufacturers, and network equipment vendors.

What 5G network challenges is 3GPP trying to address?

The 3GPP, in its 5G-Advanced (Release 18) and future releases, seeks to address challenges like:

Why is 6G wireless simulation critical?

The visionfor 6G includes complex system requirements like:

However, real-world wireless data collection is impractical until the first customer pilots — and even then, it will be expensive and time-consuming.

This is why accurate standard-compliant simulations are critical. They enable research, prototyping, synthetic data generation, and development of functional and performant 6G systems from day one.

What are some key 3GPP AI use cases?

Let's understand some key AI use cases of 5G-Advanced and 6G in more depth:

Channel estimation (CE)

For reliable communication, receivers on both ends must be able to decode the received data accurately. This is the primary goal of channel estimation.

The 5G base station (5G Node B or gNodeB or gNB) performs physical uplink shared channel (PUSCH) estimation to characterize the channel between itself and the user equipment (UE). The UE does physical downlink shared channel (PDSCH) estimation to characterize the channel from its end.

The characterization is based on pilot reference signals (RS), such as demodulation RS or sounding RS (SRS). Traditional CE applies rigid formulas like least squares or linear minimum mean square error to these signals.

However, in 5G-Advanced and 6G, high device density and dense urban environments with lots of buildings and obstacles result in severe multi-path distortions. Also, high-speed gNodeBs or UEs in drones, airplanes, and satellites must manage significant Doppler shifts. In such scenarios, the channels become highly dynamic and nonlinear.

Figure 1. Channel estimation using AI

The solution? Instead of rigid formulas, use AI for highly dynamic and adaptive CE.

Deep neural networks learn predictive patterns from a channel's key features like temporal dependencies, spatial complexity, frequency selectivity, and sparsity. Traditional estimators provide baseline estimates, which are combined with ideal channel responses (labeled data) in a supervised learning setup for the AI model. Once trained, the model does inference to estimate the full channel.

CSI prediction

Figure 2. CSI exchange between UE and gNodeB

CSI includes crucial information about channel fading, scattering, diffraction, interference, noise, and more. For determining the CSI, a UE calculates information like channel quality indicator, precoding matrix indicator, and rank indicator using the CSI reference signal (CSI-RS). Based on CSI feedback from the UE, a gNodeB adapts its modulation, coding, and beamforming to current channel conditions.

However, in scenarios like fast-moving UEs, the CSI gets outdated fast. Such channel aging severely reduces network performance and efficiency in UM-MIMO systems like 5G/6G.

Figure 3. Time-domain CSI prediction to mitigate channel aging

To mitigate channel aging, ML models are used for time-domain CSI prediction. By predicting how the channel will evolve, the CSI can be kept effectively fresh even in dynamic conditions.

CSI feedback compression

CSI is critical for many advanced features in 5G/6G that boost spectral efficiency and throughput.

As the number of antennas increases (as in UM-MIMO), the volume of CSI information becomes enormous. In the future, 6G will have hundreds or thousands of antennas. This isn't good because of:

Figure 4. CSI feedback compression using AI

In 5G-Advanced, 3GPP wants AI models that intelligently compress theCSI feedback. Unlike traditional data compression methods, these AI models leverage CSI semantics to compress raw channel data or the precoding matrix more efficiently. An encoder model on the UE compresses the high-dimensional CSI data into a compact representation. On the gNB, a complementary decoder model reconstructs the complete CSI data with minimal loss.

Training methodologies for such two-sided models, like joint training or separated training, are a key focus area for the 3GPP. Given the diversity of network operators, equipment, and UEs, ensuring model interoperability is another focus area.

Beam management

Figure 5. Beam selection steps

Beamforming is critical for UM-MIMO. However, currently, finding the best transmit-receive beam pair takes a lot of time and signals.

That's why 5G-Advanced and 6G will use AI for smarter beam selection, less searching, better connections, and faster speeds.

Figure 6. Spatial beam predictions using AI

Figure 7. Temporal beam predictions using AI

AI models will find the optimal beams faster using spatial predictions (based on nearby signal measurements) and temporal predictions (based on past beam selections).

Mobility

Figure 8. Traditional handovers in mobile networks

In traditional handovers, disconnecting from the previous tower and connecting to the new one results in a service interruption of 50-90 milliseconds.

5G-Advanced seeks to improve on this using L1/L2-triggered mobility (LTM) to reduce interruptions to 20-30 milliseconds, potentially even lower.

Figure 9. Timing of traditional handover vs. LTM

LTM benefits applications where every millisecond counts, like immersive extended reality and real-time gaming.

Figure 10. LTM

LTM involves preparing a UE in advance to contact the next candidate base station in its trajectory.

Positioning

Figure 11. Traditional positioning

Positioning accuracy in 5G New Radio (NR) is only about 3-10 meters. It relies on the time difference of arrival and multilateration using position RS and sounding RS from multiple transmission and reception points (TRPs). Accuracy degrades in poor line-of-sight (LOS) conditions and dense urban multipath environments where signals bounce around. This method can't achieve the accuracy expected by 5G-Advanced (<10 cm), let alone 6G (one cm).

Figure 12. AI for positioning

To improve accuracy, AI is used for positioning as follows:

What is the WirelessPro 3GPP AI Simulation Platform?

Figure 13. WirelessPro capabilities

WirelessPro 2026 is a cutting-edge software framework with Python and C++ components for simulating various aspects of 5G NR, 5G-Advanced, and future 6G cellular networks. Tailored for researchers, engineers, and developers, WirelessPro empowers wireless communication system engineers to model, simulate, and analyze various aspects of 5G NR, 5G-Advanced, and future 6G with unparalleled ease and accuracy.

It supports 3GPP-compliant simulations of:

The current version of WirelessPro is aligned with the 3GPP Release 18 version of March 2025.

What makes WirelessPro different from other simulation tools?

Figure 14. WirelessPro benefits

WirelessPro's unique features are outlined below:

How does WirelessPro facilitate 3GPP simulation use cases?

WirelessPro’s simulation capabilities span a variety of use cases, including:

Let’s take a closer look at how WirelessPro facilitates each one.

Supercharges channel estimation

Figure 15. WirelessPro components for CE

WirelessPro includes a reference convolutional neural network (CNN) model for PUSCH estimation and simulations based on spatial and frequency features. Scripts and tutorials for training and inference are also included.

Figure 16. Synthetic data generation for training a CE AI model

WirelessPro also generates large amounts of synthetic data required for training such AI models. It configures 3GPP-standardized channel models with diverse signal parameters to generate realistic datasets for urban and rural environments, different antenna configurations, and more.

Predicts CSI accurately

Figure 17. WirelessPro components for CSI prediction

WirelessPro provides a CNN with long short-term memory (LSTM) for CSI prediction and simulation. The CNN uses spatial features while the LSTM uses temporal features to predict the CSI accurately.

Optimizes CSI feedback compression

CSI is inherently correlated across multiple dimensions as follows:

WirelessPro provides a PyTorch-based reference transformer network implementation for CSI compression. Transformers are not doing just dumb data compression but semantically aware domain-specific compression.

For low-latency CSI encoding and decoding, WirelessPro implements optimizations like quantization and pruning.

WirelessPro supports different training approaches like:

Implements smarter beam selection

Figure 18. WirelessPro components for beam management

For beam selection and simulations, WirelessPro includes a reference deep neural network (DNN) that predicts using spatial features and an LSTM that predicts using temporal features.

Figure 19. Beam selection using AI

WirelessPro enables you to:

Simulates high-speed mobility

Figure 20. Simulate moving UEs and L1 measurements

WirelessPro supports LTM system-level simulation by supporting custom 5G network layouts, base station placement, UE distribution, and UE trajectories.

Achieves super-accurate positioning

Figure 21. WirelessPro for positioning

WirelessPro implements a reference residual network (ResNet) CNN that can be trained on 3GPP channel models to learn complex relationships between radio signals and physical locations for simulating direct and assisted positioning.

Enables AI/ML workflows

WirelessPro supports AI/ML building blocks for 5G and 6G simulations and research, including:

Sets up advanced channel modeling

WirelessPro includes building blocks for 5G-Advanced and 6G channel modeling like:

Simulates site-specific channel modeling

WirelessPro seamlessly integrates RaySim's output, enabling site-specific, high-resolution channel data as a baseline for confidently exploring advanced beamforming techniques and AI/ML-enabled NG-RAN features.

Channel Studio RaySim Tool is a high-fidelity ray tracing emulation engine that generates realistic, site-specific channel data.

Experiments with NTN channel modeling

WirelessPro supports the 3GPP TR 38.811 channel model for NTNs. It can realistically simulate satellite links with impairments like path loss, Doppler, and delay, as well as flexible options for defining satellite trajectories.

Explores 6G channel coding

For researchers exploring 6G, WirelessPro demonstrates custom channel codes like advanced low-density parity-check for data channels and polar codes for control channels.

How is Python contributing to AI-assisted designs?

The Python ecosystem, with components like the PyTorch AI framework and interactive computational environments like Jupyter, is at the forefront of AI research and implementation.

Keysight's WirelessPro uses them to provide:

Additionally, related Keysight software like Advanced Design System and SystemVue provide Python APIs for simulations, data analytics, and automated tests.

Hop on to Keysight's WirelessPro 3GPP AI simulation platform

This blog post gives 5G/6G communication system engineers and researchers a deep understanding of 3GPP AI use cases and WirelessPro's support for them.

As a leader in wireless standards and simulation technologies, Keysight's goal is to help you build trust and confidence in the results produced by our highly capable simulation tools. That's why WirelessPro will evolve in sync with 3GPP releases and emerging technologies like AI/ML. Engineers will get access to WirelessPro's comprehensive documentation, useful tutorials, helpful community groups, and responsive technical support to get the most out of WirelessPro.

Contact us for expert insights into your 3GPP AI research and development needs.

Learn more

WirelessPro 3GPP AI Simulation Platform | Keysight

W8301B WirelessPro 5G Advanced Bundle | Keysight

Bootcamp: Designing the 6G Air Interface with AI