Unlock Future Crash Header Image v01

Unlock the Future of Vehicle Crash Optimization with Reduced Order Modeling (ROM)

Advanced Reduced Order Modeling for More Effective Structural Crash Optimization

Are you an engineer looking to revolutionize vehicle design and crash simulation? Discover how Reduced Order Modeling (ROM), specifically through Keysight CAE's advanced ADMORE technology, can transform your workflow. During our Keysight CAE LIVE 2023 virtual conference, my colleague Gavin England, PMM crash and safety here at Keysight CAE and I explored innovative methods that enable faster, cost-effective, and more accurate optimization of vehicle structures. This wasn't just theory—it is a real-world application with Renault, showcasing the power of ROM in actual crash simulation scenarios.

Our partnership with Renault utilized ADMORE's cutting-edge sPGD and ReCUR methods to optimize vehicle-side member reinforcement, dramatically cutting down simulation time and costs. These methods not only streamline the process but also open up new avenues for non-specialist engineers to participate in high-level simulations, democratizing the design process.

But let’s start with clarifying some fundamental questions before we move forward.

What is the Reduced Order Modeling Approach?

Reduced Order Modeling is a mathematical technique that simplifies complex simulations by reducing the number of variables and equations needed to describe a system. Instead of solving full-scale, high-fidelity models, ROM uses a smaller set of basis functions to approximate the system's behavior. This reduction in complexity makes it possible to perform simulations more quickly and with less computational power, without significantly compromising accuracy.

What is the Role of Reduced Order Models in Product Development?

Reduced Order Models (ROMs) play a crucial role in product development and the Design of experiments (DoE) by enabling rapid prototyping and iterative design processes. They allow engineers to quickly assess the impact of design changes, material selections, and other variables on the final product's performance. This capability is particularly valuable in industries like automotive engineering, where safety standards are stringent, and time-to-market is critical.

What is the Value of Using ROM in Engineering?

The primary advantage of using ROM is its ability to significantly reduce computational costs and time. Traditional high-fidelity models require extensive computational resources, often running for many hours on high-performance processors. Reduced Order Models can achieve similar levels of accuracy with much less computational effort, making it an invaluable tool in scenarios where multiple design iterations are necessary, such as crash simulations and vehicle design optimization.

Is Proper Orthogonal Decomposition the Only Method for Reduced Order Models?

No, Proper Orthogonal Decomposition is not the only ROM method. In their presentation, Gavin and Fatima highlighted two other main methods:

How do Reduced Order Modeling, Machine Learning, and Hybrid Twin Relate to one Another?

Model Order Reduction, Machine Learning, Artificial Intelligence (AI), and the Hybrid Twin approach are interconnected concepts in the field of advanced computational modeling and simulation.

ROM provides a simplified yet accurate representation of complex system models, which is computationally efficient. Machine learning and hybrid AI enhance Reduced Order Models by enabling rapid physical insights, model predictions and early decision-making. Hybrid Twins leverage these technologies to create dynamic digital replicas of physical systems, allowing for real-time monitoring, optimization, and predictive analysis. Together, these technologies enable more effective and efficient system design, analysis, and operation.

What Are Practical Examples of Reduced Order Models?

There are plenty of use cases across industries.

Why Download Our Technical Paper on “Advanced reduced order modelling for more effective structural crash optimization”?

Are you ready to dive deeper into the world of Reduced Order Modeling and its applications in crash optimization? We have outlined the full project in a technical paper for you to understand the scope and value and make sense of project results. Here are the 3 reasons why you should download this technical paper:

  1. In-depth Technical Insights: Understand the mechanics behind reduced-order modeling and its applications in vehicle crash optimization.
  2. Real-world Application: See how we partnered with Renault to tackle real challenges in crash simulation.
  3. Cost and Time Efficiency: Learn how to achieve optimal safety and performance with fewer resources.

Join us in pushing the boundaries of what's possible in automotive engineering!

limit
3