SOS Core and Cadence Virtuoso: Modernizing Design Data Management

In the world of analog, RF, and mixed-signal IC design, few tools are as deeply embedded in engineering workflows as Cadence Virtuoso. For decades, it has served as the backbone of custom IC development, powering everything from initial schematic capture to layout implementation and physical verification. Tens of thousands of engineers rely on it daily to design the chips that drive modern electronics, from mobile devices to high-performance computing systems.

But while Virtuoso excels as a design creation environment, the complexity of modern semiconductor projects has outgrown traditional, file-based workflows. Today’s designs are larger, more interconnected, and developed by teams that are often distributed across multiple sites and time zones. In this context, managing design data is no longer a background task; it is central to the success of the entire project.

This is where Keysight Technologies’ SOS Core comes into play.

Rather than introducing yet another standalone system that engineers must learn and operate in parallel, SOS Core embeds itself directly into the Virtuoso environment. It transforms Virtuoso from a powerful but isolated design tool into a fully integrated, data-managed platform. Version control, collaboration, traceability, and workflow automation become native capabilities, accessible through the same menus and interactions designers already use every day.

The result is not just improved efficiency, but a fundamental shift in how teams collaborate, iterate, and bring designs to tapeout with confidence.

Data Management Matters More Than Ever

The increasing importance of design data management is not accidental- it is a direct consequence of how semiconductor development has evolved.

Growing Design Complexity

Modern analog and mixed-signal designs are no longer small, self-contained blocks. They are deeply hierarchical systems composed of reusable IP, parameterized cells, and tightly coupled functional domains. A single top-level design may depend on hundreds of underlying cellviews, each evolving independently.

Without structured data management, even a small change in one part of the hierarchy can have unintended consequences elsewhere-and tracking those dependencies manually quickly becomes unmanageable.

Parallel, Distributed Development

Design is no longer a linear process handled by a single engineer. Instead, it is highly parallel:

Often, these roles are distributed across different teams, sites, and countries. This introduces a critical challenge: ensuring everyone is working on the correct version of the design at the right time.

Without a centralized system:

The Limits of Traditional Version Control

Conventional software-oriented version control systems struggle in this domain because IC design data is fundamentally different:

This is why hardware design relies on check-out/check-in with locking, rather than merge-based workflows. But implementing this model outside the design tool introduces friction and inefficiency.

The Cost of Getting It Wrong

Poor data management doesn’t just slow teams down, it directly impacts product outcomes:

In advanced nodes or high-performance designs, even a minor misalignment between schematic and layout can result in weeks, or months, of delay.

The Need for Embedded, Workflow-Native Solutions

What modern design teams need is not just version control, but design-aware data management that lives inside their primary tool.

This means:

This is exactly the gap that SOS Core fills within Cadence Virtuoso.

By embedding data management directly into the design environment, it ensures that every operation-whether it’s editing a schematic, updating a layout, or reviewing changes-is inherently version-controlled, traceable, and aligned with the broader team workflow.

What Is SOS Core?

SOS Core is a streamlined, high-performance design data management platform built specifically for engineering teams. It delivers enterprise-grade capabilities without the overhead typically associated with large PLM or version control systems.

At its core, SOS provides:

The result is a system that prioritizes performance, simplicity, and traceability—all critical for hardware design teams.

Deep Integration with Cadence Virtuoso

Unlike bolt-on solutions, SOS Core is deeply embedded into the Virtuoso environment.

Once configured, it extends Virtuoso through:

Engineers can perform all essential data management tasks- check-in, check-out, update, diff, tagging-without ever leaving Virtuoso.

A Natural Designer Workflow

One of the strongest aspects of the SOS–Virtuoso integration is how  natural  it feels.

Designers don’t need to learn a new system, they simply continue using Virtuoso as usual.

A Typical Daily Flow

  1. Open a cellview → Auto checkout prompt appears
  2. Edit and save locally
  3. Run simulations (Spectre, DRC, LVS, etc.)
  4. Check in changes with a description and optional tag
  5. Update workspace to sync team changes

Everything happens inside Virtuoso. No context switching. No manual syncing.

Visual Design Diff (VDD): A Standout Feature

Visual Design Diff (VDD) is one of the most impactful capabilities of the SOS Core integration, addressing a long-standing challenge in IC design: understanding what actually changed between design revisions. Traditional comparison methods—whether manual inspection or file-based diffs—offer limited insight into schematic and layout data, where meaning is tied to structure and connectivity rather than text.

VDD brings this analysis directly into Cadence Virtuoso, transforming it into a visual and design-aware experience. Engineers can compare two revisions or cellviews side by side, with changes highlighted directly on the canvas. Added, removed, and modified elements are clearly marked, making it easy to grasp differences at a glance rather than interpreting abstract reports.

Alongside the visual view, a structured Differences Browser organizes changes by type—such as instances, nets, or properties—and allows quick navigation to specific areas of interest. This combination of visual highlighting and structured navigation enables fast, focused analysis without scanning entire designs.

What sets VDD apart is its awareness of design intent. In schematics, comparisons are based on electrical connectivity rather than geometry, ensuring that purely cosmetic edits do not appear as functional changes. In layouts, VDD performs efficient layer-based comparisons directly on OpenAccess data, avoiding the need for external GDSII workflows while still delivering precise geometric analysis.

VDD also scales to hierarchical designs, allowing engineers to analyze changes across entire design trees with filtering options to suppress irrelevant differences. In practice, this makes design reviews more efficient, debugging more direct, and collaboration more transparent.

By turning complex design differences into clear, visual insight, VDD helps teams move faster while maintaining confidence in the integrity of their work.

Final Thoughts

The integration of SOS Core with Cadence Virtuoso represents far more than the addition of version control features to an existing design environment. It fundamentally changes the way engineering teams interact with design data, embedding collaboration, traceability, and workflow management directly into the tools engineers use every day.

It turns Virtuoso into more than a design tool, it becomes a fully data-managed engineering platform.

Key benefits include:

For analog and mixed-signal design teams, SOS Core is not simply an add-on to Virtuoso—it is a foundational enhancement to the engineering process itself. By transforming Virtuoso into a fully data-managed design platform, SOS Core enables teams to collaborate more effectively, manage complexity with confidence, and move from design concept to tapeout with greater speed, visibility, and control.

To learn more: download the application note or visit the webpage.

Try SOS Core for free

Related Posts

limit
3