A transparent car with wheels AI-generated content may be incorrect.

Revolutionizing Comfort: How Simulation is Transforming Automotive Seat Design

You might not think it, but in the world of automotive design, few components are as critical—and as complex—as the seat. It’s where drivers and passengers spend every moment of their journey, and it must deliver on multiple fronts: comfort, safety, durability, and style. Traditionally, achieving this balance required countless prototypes, physical tests, and iterative redesigns. But now, automakers and their seat suppliers are relying on simulation software to design and test seats that meet the standards required by today’s passengers.

This blog will take a look at the challenges and considerations that manufacturers are facing, and where simulation can make a difference in ensuring everyone in the vehicle will be both comfortable and safe.

Regulatory Compliance for Automotive Seat Design

Vehicle seats must comply with a broad array of international safety regulations, such as FMVSS in the United States, ECE standards in Europe, and GB standards in China. Meeting these differing regulatory requirements often leads to the development of multiple design variants for a single seat platform. Compliance involves rigorous testing procedures, but these evaluations increase both development time and cost, making regulatory compliance a significant design and engineering hurdle.

Which is why seat engineers/designers are using simulation software to help overcome some of these hurdles…

Simulation as a Strategic Tool in Seat Design and Validation

Simulation software uses geometry and material properties to create predictive seat models capable of evaluating all key performance metrics—including static, dynamic, and thermal comfort, as well as crash and safety performance—through a multiphysics approach.

This supports seat manufacturers throughout the entire development process, from the definition phase—where it aids in design decisions such as material selection and structural layout—to the validation phase, where it simulates real-world performance under various loading and environmental conditions.

By enabling rapid iteration and early detection of design issues, simulation significantly reduces the need for costly physical prototypes, shortens development timelines, and supports compliance with regulatory standards. It also helps drive innovation by allowing engineers to explore a wider range of design alternatives with minimal risk, ultimately delivering seats that are more comfortable, safer, and better optimized for diverse occupant needs.

7 Seat Design Factors and the Impact of Simulation software

Here are just some of the considerations that seat designers need to consider, and where simulation software can play its part:

1. Ergonomics and Comfort

Here, simulation enables designers to model the seat shape, foam layering, and adjustability features to evaluate posture support and occupant fit. It can simulate pressure distribution across the seat surface, helping to fine-tune lumbar support, thigh bolstering, and seat height to reduce fatigue on long drives. Virtual models also allow for quick testing of various adjustment mechanisms and cushioning materials—such as memory foam or multi-density layers—to find the right balance between softness and support before physical prototyping.

2. Safety Requirements

Simulation is essential in assessing crashworthiness by replicating crash scenarios to evaluate how a seat absorbs energy and protects occupants. It can model the structural response of seat frames and cushions under impact.

3. Materials

Virtual testing tools allow engineers to evaluate how different materials used for upholstery, foams, and structural components respond. Fatigue simulations can predict wear and deformation in foam padding, while thermal models help with comfort analysis. Designers can compare frame materials like high-strength steel and aluminum to optimize for weight.

4. Manufacturing and Assembly

Simulation software supports manufacturability by enabling early assessment of design feasibility and assembly complexity. Virtual models can test modular configurations, helping ensure compatibility across vehicle variants. Designers can simulate production processes—such as fabric trimming or foam molding—to identify potential issues such as unexpected wrinkles and reduce cycle time. Cost and quality implications or fabric tension can be explored and resolved before physical builds, improving both efficiency and product quality.

6. Sustainability

By modeling new eco-friendly materials, such as plant-based foams or recycled fabrics, simulation helps assess their impact on comfort without the need for extensive physical testing. It also enables the design of seats with end-of-life considerations, evaluating how easily components can be disassembled and materials separated for recycling.

The Smarter Way to Design and Validate Car Seats: Keysight’s Virtual Seat Solution (VSS)

The Virtual Seat Solution (VSS) from Keysight, is a powerful finite element simulation tool tailored specifically for seat modeling. Unlike standard FE software, VSS combines high-level simulation capabilities with an intuitive, guided workflow that makes it accessible—even to engineers without deep experience in finite element analysis. The tool simplifies model creation by walking users through automated steps, such as selecting seat components (covers, foams, etc.) and assigning material properties using an embedded database when needed. Once a model is built, VSS makes it easy to iterate on design—users can, for example, morph cushion shapes to resolve issues like pressure peaks or add thermal modeling by importing geometry, meshing, and projecting heating elements. The result is a multiphysics model capable of simulating seat performance in terms of static and dynamic comfort, vibration, and thermal behavior.

Beyond comfort simulation, VSS also plays a key role in simulating seat manufacturing, adding value during both the design definition and validation phases. In the definition phase, VSS helps assess manufacturability by generating cover flat patterns from the 3D seat shape and determining foam mold geometry within minutes using its graphical interface. During validation, VSS evaluates potential manufacturing defects and enhances model realism by capturing residual stresses between the seat cover and foam—factors that significantly influence H-point calculations and pressure distribution in later simulations.

Its integrated, user-friendly approach accelerates development, increases simulation accuracy, and helps manufacturers deliver seats that are not only manufacturable but also safer, more comfortable, and tailored to a diverse range of users.

Altogether, VSS delivers a comprehensive, validated platform for optimizing seat design from early concept through final validation.

For more information visit the dedicated VSS webpage.

Related Posts

limit
3