Person working at a laptop with software projected in background

Using Example Models in CODE V

What are CODE V example models and how are they useful?

Did you know that you can quickly learn specific features of CODE V using example models?

Each example model includes a PDF document that explains the feature you will learn, describes the example model, and provides step-by-step instructions for using the example model.

Many examples also include a sequence (.seq) file that documents all the steps and analysis results. This gives you flexibility to learn a CODE V feature either by using the graphical user interface (GUI) as described in the PDF, or by using the Macro-PLUS programming language in the sequence file.

How does this work?

To understand how to use CODE V example models, we’ll focus on the Beam Synthesis Propagation (BSP) example, BSP_BallCouple. This example demonstrates how to set up Pre-Analysis for a ball couple lens. The steps in the included PDF show you how to set the output you need for the BSP analysis.

An excerpt from a PDF with a CODE V GUI screenshot and instructions walking the user through two steps for outputting 2D intensity plots.

Figure 1. Step-by-step instructions walk you through selecting output settings.

Additional steps guide you through the process of selecting the appropriate sampling and image patch size. By the time you get to the last step, you will be able to use BSP to calculate the image intensities correctly.

An excerpt from a PDF with two CODE V screenshots and an explanation of intensity plots on a smaller area.

Figure 2. Further details on intensity plots.

With the example models, you will explore CODE V’s extensive design and analysis capabilities as you work on practical examples. You can quickly learn how to use a feature and be instantly more productive. Get a head start designing your next imaging application with the example models in CODE V.

limit
3