Texture suggesting a data center

Metalenses: The Next Revolution in Optical Technology

Do you know what metalenses are? Metalenses can control light by its surface properties and can be flat and thin. Spherical aberrations are not an issue and these special lenses can replace bulky curved lenses. This has the potential to reduce the number of lenses in a system and create compact lens systems for imaging, sensing, and display applications.

A few years ago, Samsung combinedmetalenses and refractive lenses to develop a smartphone camera sensor surpassing 100 megapixels. LG developed an ultrathin camerametalens for self-driving electric vehicles. Metalenses pave the way for drastic miniaturization of imaging systems like electric vehicle cameras, and they can also be used in phones and various other micro-camera applications. In addition, researchers in the United States used a common semiconductor manufacturing process to produce a large aperture, flat metalens. It was used as the objective lens in a simple telescope, and it achieved superior resolving power and produced clear images of the surface of theproduced clear images of the surface of themoon.

Though metalenses are a promising advance in scaling down the size of optical systems, there are challenges, both in designing them and manufacturing them to scale.

One challenge with metalenses is designing a metalens with millions of variable subwavelength unit-cells, called meta-atoms. To modulate light locally and coherently requires design experience and a deep understanding of fundamental physics. Metalens designs involve defined lens phase profiles, a meta-atom library, and layout of the meta-atoms on the metalens surface. Then, the optical designer must choose an approach to simulate the built metalens to evaluate its performance.

If manually designing a metalens, the approach relies on a pre-defined phase profile, which is valid for a fixed incident condition only because the transfer function of the meta-atoms varies at different wavelength, incident angle, and polarization. Therefore, a phase profile optimized at a particular incident condition is not valid at others. As a result, it is very difficult to design a metalens with multiple functions, such as an achromatic lens for a wide spectral range or a large field of view (FOV) lens for wide incident angles.

Could there be a user-friendly design tool to automate metalens design for engineers to design metalens systems quickly and easily? Though significant efforts have been made worldwide to develop automation flows with inverse design capabilities, Keysight Optical Design Engineering has developed the first fully automated commercial tool, MetaOptic Designer, that provides inverse design capabilities for metaoptics. The optimization algorithm employs the well-known adjoint method, which can easily handle millions of design variables.

To design a metalens in MetaOptic Designer, the user specifies the set of lenses in the optical system and the bidirectional scattering distribution function (BSDF) database for each, as well as the desired target patterns and focus lengths. Then, the tool determines the design parameters across each metasurface and exports Graphic Data System (GDS) and optimization results, shown in Figure 1.

Target pattern, optimized pattern, and optimized layour in MetaOptic Designer

Figure 1. MetaOptic Designer overview

Now, optical designers can have a dramatically simplified and speedier design workflow when designing a metalens, with minimum inputs required.

Will metalenses revolutionize the industry? Lead researcher Xingjie Ni at Pennsylvania State University believes that metasurfaces can be a game changer in optics, because their unprecedented capability for light manipulation makes them powerful candidates for next-generation optical systems. On a nanoscale, ametalenshas also been used to focus vacuum ultraviolet light on a small spot less than 2 microns in diameter from intricate nanostructures with a zinc oxide thin film.

There’s no question that there will be a demand for compact lens systems and that many more designs will incorporate metalenses. Now, we’re paving a way for designers at all levels of expertise to create novel metalens designs quickly and easily, with accurate optimization results.

limit
3