Minimizing Driver’s Range Anxiety with System Level Simulation of Electric Vehicles

Improve range prediction, passenger comfort and overall energy efficiency

On-Time and Flawless Delivery

Lara, an experienced transporter for a cold storage packaging company primarily operating in Germany, undertakes three weekly trips between Munich and Dresden. Her role involves delivering frozen products between city warehouses, requiring strict adherence to timely deliveries while maintaining the payload at a constant temperature of -20°C.

To support sustainability goals and minimize environmental impact, the company recently transitioned from conventional trucks to electric-powered trucks. This shift aims to improve ratings on low emissions and reduce carbon footprints, reflecting a modern, eco-conscious approach.

While Lara is confident in her driving abilities and her track record of punctual deliveries, the switch to electric trucks introduces new challenges. She now faces the need to adapt to the logistics of charging and recharging the vehicles during trips. This adjustment fuels her "range anxiety," a common concern in the electric vehicle (EV) industry, which may directly influence her performance and the overall efficiency of the company she represents.

Addressing Range Anxiety: Overcoming a Key Challenge for Electric Vehicle Adoption

Article content

Range anxiety is a significant factor influencing consumer confidence in adopting EVs. While the shift from internal combustion engine (ICE) vehicles to EVs has gained substantial momentum in recent years, this transition brings with it a mix of excitement and apprehension. Automakers are increasingly committed to putting more EVs on the road, yet consumers remain concerned about the infrastructure needed to support this change.

A consumer's decision to adopt and embrace EVs often hinges on several pressing questions:

These questions, compounded by the overwhelming amount of information available online about battery-powered vehicles, often complicate the decision-making process.

The anxiety surrounding EV range stems from these uncertainties. To alleviate this concern, automakers must leverage advanced engineering and cutting-edge technology to provide precise range estimates. This not only reduces drivers’ apprehension about range but also enhances their overall driving comfort and experience, paving the way for broader EV adoption.

Factors Influencing EV Range Predictions

Largely the battery capacity and the overall energy consumption should help to predict the range better. However, even if you know the exact battery capacity, the energy consumption can vary depending on multiple influencing factors. Let us understand them quickly

Battery capacity and overall energy consumption are critical for predicting an EV's range. However, even with precise knowledge of the battery capacity, energy consumption can vary significantly due to several influencing factors. Let’s explore them:

Article content

All these factors exhibit nonlinear and dynamic interdependencies. A system-level analysis of these variables—and others like them—enables designers and engineers to enhance transparency and make more accurate range predictions.

The Impact of Colder Temperatures on EV Range

Colder climates present unique challenges for EV range performance. Cold air is denser than warm air, causing increased aerodynamic drag, and additional energy is required to heat the cabin. Heat pumps in EVs must work harder to manage heat transfer effectively, further impacting energy consumption.

Countries like the Nordics, with high EV adoption rates, offer ideal proving grounds to test EV range performance in freezing temperatures. For example, the El Prix Winter Range Test, held in January 2025 in Norway, assessed 24 brand-new EVs. Each vehicle was fully charged and driven on the same hilly route until it ran out of energy. The test compared advertised WLTP ranges with real-world distances, providing valuable insights into how weather and terrain affect performance.

Article content

Source: Eirik Aspaas / © NAF

Highlights from the Test Results

Here are the top 5 EVs that performed best in the test. The full results can be viewed on the Motor.no website. Source: NAF Elbil Test and Motor.no

Article content

Interestingly, the Tesla Model 3 fell short of expectations, showcasing how real-world conditions can defy expectations set by manufacturers.

The Role of Early Design Phase Testing

What if EV range and energy consumption patterns could be simulated at the system level during the design phase? This approach could potentially provide more accurate predictions of range performance under harsh or extreme conditions, helping engineers address these challenges proactively.

Would such early-stage analysis revolutionize how we design and market EVs?

Modeling an Electric Vehicle in SimulationX

Article content

Electric Truck Model in SimulationX

We created an electric truck model in SimulationX as shown in the picture above using the Vehicle Drive Library. This demonstrator focuses on testing the battery range for the truck vehicle running on the same route but in different weather conditions. Below are some of the key components of this model:

Converting Lara’s range anxiety into improved decisions & on time payload delivery

In the beginning of the article, we spoke about Lara, an experienced transporter for a cold storage packaging company and her dilemma with electric trucks. When automotive manufacturers have designed their electric trucks with full control and transparency over the actual delivered on-road electric truck, then the overall customer’s experience around range anxiety or EV adoption becomes a confident approach. We’re happy to say that Lara now loves to drive her new trailer with accurate range predictions in varying weather and hilly terrain or highways. She knows exactly how long the charge will last, when to re-charge, how long to charge and ensure the payload delivery on time. She is also quite proud that her small contribution towards adoption of greener and cleaner vehicle is making a huge environmental impact inspiring a lot of her other colleagues.

To learn more about system level simulation and SimulationX visit the webpage

Related Posts

limit
3