Enhancing Optical System Design with Advanced Stray Light Analysis Tools
Stray light can significantly impact the performance of optical systems, leading to unwanted artifacts and reduced image quality. Addressing this issue requires sophisticated tools and methodologies to analyze and mitigate stray light effects. In this blog post, we’ll explore the capabilities of LightTools software for stray light analysis, including ghost image analysis, sequence ray tracing, and practical examples of their application.
What is stray light?
Stray light is unwanted radiation that disrupts an optical system's performance. Whether it’s caused within the system or by external sources like the sun, stray light degrades image quality by reducing contrast and color accuracy in the final image.
Stray light can be categorized into two types: ghost images and glare (also referred to as flare or veiling glare). Ghost images are typically caused by multiple reflections between imaging components and filters, leading to secondary images that degrade the quality of the primary image. In contrast, flare and veiling glare are caused by bright light sources within or outside the field of view, which create scattered light that reduces image contrast and color fidelity.
The example in Figure 1 shows how stray light can deteriorate image quality. In this case, a bright off-axis source just outside the camera’s view creates flare as light reflects off the mechanical mounts.
Stray light analysis in LightTools
Without proper simulation and analysis tools, stray light analysis can be a cumbersome process. LightTools offers robust features, such as accelerated ray tracing with multi-threading and cluster simulations, ray paths, and sequence trace.
LightTools helps you observe the ray paths in your system for a given number of maximum hits on each surface, then isolate paths according to power, peak irradiance, and number of rays.
By identifying the specific surface interactions that create ghost images, ray path analysis enables targeted solutions — such as optimized anti-reflective coatings or surface treatments — to minimize reflections and maintain image clarity.
Enhanced results using sequence ray tracing
Sequence ray tracingray tracing in in LightTools enhances the efficiency of stray light analysis by allowing you to select specific ray paths. This technique focuses computational resources on paths of interest, enabling higher-fidelity images and faster simulations. By isolating paths, you can achieve more accurate results and better understand the behavior of stray light within the optical system.
This method is particularly useful for complex systems where traditional ray tracing methods might be computationally prohibitive. With sequence ray tracing, you can conduct detailed analyses in a fraction of the time. Figure 3 shows the use of sequence tracing to enhance a stray light path.
Figure 3. Surface sequence definition identified after the first simulation
Figure 4. Ray path interacting with a reflective mechanical mount and causing stray light
Figure 5. Resulting stray light pattern on the image sensor
Figure 6. Stray light patterns on the car scene
Additionally, LightTools software integrates with our image simulator ImSym to provide a more comprehensive analysis. The integration with the Stray Light Scanner feature provides understanding of how stray light behaves in real-world scenarios and enhances simulation accuracy. By combining ImSym with LightTools, you can simulate the impact of various environmental factors on stray light and develop more robust optical systems.
Conclusion
LightTools offers a comprehensive set of features for precise and efficient stray light analysis, enabling improved optical system performance. With ray paths, sequence ray tracing, and other advanced features, LightTools addresses stray light issues with high-quality imaging simulations that identify ghost images and flares in complex scenes.
Integrating ImSym and the LightTools’ Stray Light Scanner further enhances image analysis by incorporating scatter effects. These tools provide valuable insights into model performance, allowing designers to make informed decisions and achieve significant improvements in image quality and system performance.
Ready for the next step? Contact us today for a demo or trial.