Blog: From Mission Requirements to Validated Imagery: A Digital Workflow for Aerospace Imager Design Picture shows a mounted camera

From Mission Requirements to Validated Imagery: A Digital Workflow for Aerospace Imager Design

Modern aerospace imaging systems face a difficult challenge: they must deliver reliable image performance under demanding operating conditions long before engineers have access to physical hardware.

Design teams are expected to balance several competing requirements, including:

Optimizing a single subsystem is rarely enough. The final image is influenced by decisions made across the entire engineering workflow.

Start with the Image, Not the Lens

Aerospace imaging programs rarely begin with an optical prescription. They begin with a mission objective.

Engineers may need to:

The challenge is translating those objectives into measurable engineering requirements. Resolution, field of view, detector characteristics, optical performance, environmental behavior, and calibration requirements all emerge from the original mission need.

Overview of a dam from an Earth observation system

Figure 1. Looking for a vehicle as an Earth observation system example. Image credit: https://map.openaerialmap.org.

The most successful programs maintain that connection between mission intent and engineering decisions throughout development.

Architecture Decisions Matter More Than Many Engineers Realize

Before a detailed optical prescription exists, engineers can already begin evaluating system architectures.

Questions such as aperture  and obscuration  size, focal length,  resolution requirements,  detector format, packaging constraints, and optical configuration have long-term consequences. The goal is not simply to find an optical design that performs well on paper and meets a requirements specification, but to identify a design that can be manufactured, integrated, tested, and operated successfully.

Digital trade studies make it possible to compare:

Simulation allows engineering teams to evaluate both quantitative performance and representative imagery before committing to a particular approach.

Stray Light Should Not Be a Late Discovery

Stray light analysis is often treated as a downstream activity. By that stage, major design decisions may already be difficult to change.

Potential sources of unwanted light include:

A digital workflow enables engineers to identify dominant contributors earlier and evaluate mitigation strategies before hardware is built, and understand the effects that required baffling will have on performance..

Rather than becoming a troubleshooting exercise, stray light analysis can become part of the initial complete  design process, from zero order direct path mitigation to multi-bounce paths.

Optical simulation diagrams and screens

Figure 2. Automated source scans reveal critical angles and image artifacts

The Detector Is Part of the System

Detector selection cannot be separated from the rest of the imaging chain.

Key sensor characteristics include:

The real question is not which detector looks best on a specification sheet.

The real question is whether the detector helps the system satisfy its mission requirements.

When detector models are evaluated alongside optics, scene content, and imaging conditions, engineering teams gain a more realistic understanding of overall performance.

The Final Validation Happens in the Image

Metrics such as MTF, SNR, distortion, and irradiance remain essential throughout development.

However, the final measure of success is straightforward:

Can the system produce the image needed to accomplish the mission?

Image-domain simulation helps answer that question by combining:


into a single evaluation environment. 

This approach makes it easier to understand how design decisions affect the imagery that operators, analysts, or automated systems will ultimately use.

Unobscured up to 50% Obscured real-world dam scenes, with corresponding test target images, and minimum optical MTF

Figure 3. Ideal lens optical performance (MTF and real-world dam scene)

Raw images compared to post-processed images

Figure 4. Compare the real-world images with our system performance metrics (picking the SNR / MTF operating point against spec)

Building a Connected Digital Thread

The most effective aerospace imaging workflows connect every stage of development:

  1. Define the mission objective
  2. Allocate system requirements
  3. Explore architecture alternatives
  4. Develop the optical design
  5. Evaluate stray light and opto-mechanical effects
  6. Select and model detectors
  7. Simulate the resulting image
  8. Verify performance and iterate

By maintaining this digital thread, engineering teams can identify issues earlier, evaluate alternatives more efficiently, and reduce reliance on costly physical iterations.  Using ODE tools, you have a connected digital thread for continuous optimization from requirements to validation. Define mission -> Allocate requirements -> Design optics -> Model mechanics and stray light -> simulate complete image -> Verity and iterate -> Back to Define mission Figure 5. Build a connected digital thread.

Key Takeaway

Aerospace imagers are not defined by optics alone. They are the result of complex interactions between mission requirements, optical design, detectors, mechanics, environmental conditions, calibration processes, and image processing.

A connected digital engineering workflow helps teams:

The result is not simply a better optical design. It is a better understanding of how the complete imaging system will perform when it matters most.

limit
3