Machine vision system using ImSym - Imaging System Simulator to inspect screws on an assembly line

Optics on the Assembly Line: Design Complete Machine Vision Systems with ImSym

Machine vision systems are essential for automating inspection and quality control processes in manufacturing. These systems rely on precise optical designs to capture and analyze images of products, ensuring accuracy and efficiency.

ImSym – Imaging System Simulator is a unified platform to design, simulate, and optimize machine vision systems virtually. By modeling the entire imaging process, ImSym enables engineers to identify potential challenges, test configurations, and refine designs before physical prototypes are built.

This article explores the fundamentals of machine vision, the process of modeling such systems, and how you can use ImSym to simulate and improve optical designs for assembly line applications.

About machine vision

Machine vision systems are integral to modern manufacturing, enabling automated inspection, measurement, and sorting of products. These systems typically consist of a camera, a lens system, and a lighting setup that work together to capture high-quality images of objects on an assembly line.

The captured images are processed using algorithms to detect defects, measure dimensions, or identify specific features. For example, in an assembly line for screws, a machine vision system can replace human inspectors by using a camera to capture images and image signal processing algorithms to verify the screws’ quality.

Applications for machine vision extend beyond manufacturing. They are used in recycling centers to sort materials, in pharmaceutical production for quality control, and even in agricultural supply chains to inspect produce. The versatility of these systems makes them indispensable across industries.

Designing an effective machine vision system presents several challenges:

How do you model a machine vision system?

Modeling a machine vision system involves simulating the entire imaging process, from the scene object to the final image. This includes:

By creating a virtual prototype of the system, engineers can test different configurations, identify potential issues, and optimize performance before building a physical prototype. This approach saves time and reduces costs, making it an essential step in the design process.

Illustrated end-to-end machine vision model starting from scene object to final image Figure 1. Example of end-to-end model

Modeling the optical system with ImSym

Description of the optical system

ImSym provides a unified simulation environment for designing and testing optical systems. For example, in a machine vision system designed to inspect PCBs, the optical system includes:

ImSym integrates seamlessly with CODE V and LightTools, enabling accurate radiometric simulations and optical modeling. Engineers can import lens designs, define sensor properties, and simulate the entire optical system within a single platform.

Optical system diagram analyzing a PCB using LightTools and CODE V Figure 2. Description of an optical system that is analyzing a PCB

Image simulation

ImSym simulates the light rays traveling through the optical system, from the scene to the sensor. This includes:

For example, in a PCB inspection system, ImSym can simulate how ambient lighting and a light bar affect the visibility of holes in the PCB. By adjusting parameters such as lighting angle or sensor settings, engineers can optimize the system for better detection.

Constraints with specular reflection

One common challenge in machine vision systems is specular reflection, where light reflects off shiny surfaces and saturates the sensor. This can obscure critical features, such as holes in a PCB.

ImSym allows engineers to simulate these effects and test different solutions, such as:

Image sequence showing ImSym simulations under varying illumination angles Figure 3. Image results in ImSym from different angles of additive illumination lights

For example, a simulation may reveal that certain lighting angles cause specular reflections that obscure some holes in a PCB. By testing alternative lighting setups in ImSym, engineers can identify the optimal configuration without costly physical prototypes.

Conclusion

ImSym is a powerful tool for designing and optimizing machine vision systems. By enabling virtual prototyping, it helps engineers identify potential issues, test different configurations, and refine designs before building physical prototypes. This not only reduces development costs, it accelerates time-to-market.

Whether you’re working on assembly line automation, medical imaging, or other optical applications, ImSym provides the tools you need. Its integration with CODE V and LightTools ensures accurate simulations, while its flexibility supports collaboration across engineering teams.

Ready to take the next step? Contact us today to request a trial and experience the capabilities of ImSym.

limit
3