Designing LIDAR on a Chip: A Multiphysics Simulation Workflow for Integrated Photonics
Introduction
LIDAR (Light Detection and Ranging) has become a cornerstone technology for autonomous vehicles, enabling high resolution spatial mapping and object detection. As the industry pushes toward scalable, cost-effective solutions, LIDAR on a chip has emerged as a compelling alternative to traditional mechanical systems. Its advantages—compactness, robustness, and the absence of moving parts—make it an excellent candidate for large volume manufacturing.
However, achieving commercially viable on chip LIDAR requires careful optimization. Designers must minimize insertion loss, maximize output optical power, broaden beam steering range, and narrow the emitted beam. To meet these challenges, reliable and specialized photonic simulation tools are essential for reducing development cycles and ensuring high performance designs.
Overall Design and Simulation Strategy
To efficiently design a LIDAR-on-chip system, the device is decomposed into functional blocks, each simulated using the most appropriate tool from the RSoft Photonic Device Tools suite:
- Cascaded 1×32 splitter: BeamPROP BPM™
BPM is ideal for 1×2 splitters due to little backward reflection and suitability for slowly varying structures. - Thermo-optical phase shifter: BeamPROP BPM™ + Multiphysics Utility
BPM handles optical propagation, while the Multiphysics Utility computes temperature dependent refractive index perturbations. - Emitter (grating antenna array): FullWAVE FDTD™
FDTD (Finite Difference Time Domain) is required for omnidirectional light propagation and accurate grating coupler modeling.
This modular approach ensures each component is optimized using the most accurate and computationally efficient method available.
Fig. 1: The overall design is composed of a splitter tree that could use either MMI or Ybranch splitters, then a thermo-optical phase shifter, and finally a collection of antennas for the emitter.
Step-by-Step Design of Individual Components
Power Splitter
A splitter tree is constructed using cascaded 1×2 splitters—either MMI or Y‑branch designs.
- 1×2 MMI splitters
- Low insertion loss (~0.3 dB)
- Robust to asymmetric input
- More complex to design
- Wavelength sensitive, limited bandwidth, polarization dependent
- Y‑branch splitters
- Simple geometry (two S‑bends)
- Broadband and polarization independent
- Higher insertion loss (~2 dB)
- Less tolerant to asymmetric input
Both structures are well-suited to BeamPROP BPM, which solves one-way wave equations under assumptions of slow structural variation and monochromatic excitation.
Fig. 2: Side-by-side comparison between MMI splitter and Ybranch.
After optimizing width and length using 2.5D (2D‑EIM) BPM, sensitivity analyses were performed for symmetric and asymmetric inputs. The final 1×32 splitter tree uses four levels of 1×2 MMIs, followed by a fifth level of Y‑branches where MMIs became too large to fit the remaining layout area.
Fig. 3: Overall cascaded splitter with 1×32 branches.
Thermo-Optical Phase Shifter
Silicon’s strong thermal sensitivity (dn/dT = 0.00024/K) enables phase tuning by heating waveguide arrays. Unequal heating introduces phase delays between channels, steering the output beam.
The workflow:
- Thermal diffusion equation solved to obtain temperature distribution.
- Temperature profile converted into refractive index perturbation.
- BPM simulates optical propagation to compute amplitude and phase at the output.
- Far‑field analysis reveals the resulting beam steering.
For a temperature change of ΔT = 50 °C, the phase difference between adjacent waveguides is 120°. BPM predicts a steering angle of 15°, matching the theoretical value:
Emitting Gratings
To efficiently outcouple light (orthogonally) with minimal divergence, the grating must be properly apodized. FDTD optimization yields an optimal tapered width grating profile, normalized to the grating length (Fig. 5).
Fig. 5: Optimized grating and emitted field
Full 32‑channel FDTD simulation is computationally prohibitive (≈100 GB RAM few days’ computation time). Instead, each waveguide input is simulated independently over a large domain (5-waveguide widths). The total near‑field is obtained by coherently summing all individual near‑fields (Fig. 6b), and the far‑field is computed from its transform (Fig. 7).
Fig. 7: Emitted far-field
In figure 7, the firstorder diffraction angle is approximately 49°, closely matching the theoretical prediction:‑order diffraction angle is approximately
Conclusion
RSoft tools provide a powerful and flexible environment for designing integrated photonic LIDAR systems. Because no single simulation method can accurately model every component, decomposing the device into functional blocks—and applying BPM, FDTD, and Multiphysics solvers where appropriate—is essential.
By combining FDTD for complex radiative structures with BPM for guided wave components, designers can thoroughly analyze system level performance while optimizing each building block for maximum efficiency.
If you’re exploring integrated LIDAR architectures or evaluating photonic design workflows, feel free to ask about trial access to these simulation tools so you can experiment with your own designs.