Photograph of a crescent moon showing detailed surface craters and texture against a black sky. The illuminated portion forms a curved, bright crescent on the right side, highlighting lunar topography.

To the Moon and Beyond: The New Technologies Bringing Lunar PNT Closer to Reality

Space exploration history was made in March 2025, when Firefly Aerospace’s Blue Ghost lunar lander became the first commercial vehicle to land successfully on the Moon’s surface.

On board were ten NASA payloads deployed to collect data and samples used to plan further missions to the Moon and beyond. As those plans develop, a critical component is the ability for vehicles and astronauts to navigate effectively to, from and on the Moon.

The resulting investment in lunar PNT services is delivering new breakthroughs across the industry — from receiver design to PNT infrastructure and simulation capabilities.

Pushing the boundaries of Lunar PNT

To discuss those developments, Keysight presented a recent Inside GNSS webinar along with Samuele Fantinato, head of navigation technologies at QASCOM, and Masaya Murata, lunar PNT and LEO PNT lead at the Japan Aerospace Exploration Agency (JAXA).

Here are some highlights from that discussion.

LuGRE acquires GNSS signals on the Moon’s surface

One of the ten payloads on the Blue Ghost lander was the Lunar GNSS Receiver Experiment (LuGRE), a joint initiative between NASA and the Italian Space Agency (ASI).

LuGRE is a high-sensitivity GNSS receiver designed and developed by QASCOM, with the aim of characterizing the potential for GNSS signal reception on the Moon.

Samuele Fantinato shared some of the fascinating results from those experiments, showing how LuGRE acquired GNSS signals for the first time both  in lunar orbit  and on the Moon’s surface.

LuGRE captured the received signals as IQ files, and these are expected to be made publicly available in October 2025 — an exciting prospect for realistic lunar GNSS simulation.

New developments in dedicated lunar PNT services

However, GNSS signals alone are not sufficient for reliable lunar navigation, and an international program is underway to develop interoperable PNT services for deployment into lunar orbit.

Under the banner of LunaNet, the first mission will include four satellites in orbit around the Moon, including NASA’s LCRNS, the European Space Agency (ESA)’s  Moonlight LCNS system  and JAXA’s Lunar Navigation Satellite System (LNSS).

Masaya Murata showed how all three systems will broadcast the standardized Augmented Forward Signal (AFS), which will broadcast in the S-band frequency range for a number of reasons, including:

That’s bringing new simulation challenges to developers of lunar PNT infrastructure—a challenge which JAXA is addressing with Keysight’s PNT X simulator, which generates authentic AFS signals in line with the current LunaNet Interoperability Specification (LNIS).

Advances in lunar PNT simulation capabilities

Simulating future LunaNet signals is just one of many lunar PNT development requirements that Keysight has been working hard to address in its PNT X simulation platform. Keysight gave an update on some of the other key challenges and how Keysight is resolving them, including:

Simulating realistic lunar missions with Keysight PNT X

To show how Keysight can simulate realistic signal effects on the Moon’s surface, the webinar demonstrated how the 3D environmental modeling capabilities of PNT X to realistically recreate the topography of the Shackleton Crater near the lunar South Pole.

To this environment Keysight added simulated AFS signals from four orbiting satellites and trajectories for different rover missions — a short one of 400m and a longer one of 4 km. The team characterized signal reception in three scenarios with differing constraints, including altitude of the rover and geometric dilution of precision (GDoP).

Simulations like these provide insight into how lunar vehicles will experience PNT signals in different scenarios, enabling space agencies and technology developers to plan missions and design new technologies with confidence.

limit
3