Turn Recorded RF into Controllable Scenarios for Lab Testing
New software tool decomposes live RF recordings into discrete, controllable signals for unprecedented realism in lab-based GNSS simulation.
The ability to record and replay the live GNSS signal environment has long played a key role in testing the positioning, navigation and timing (PNT) capabilities of chipsets and devices.
GNSS record and playback systems (RPS), like the Keysight GSS6450, enable a real-world RF environment to be recorded and repeatedly replayed to a device under test (DUT). This allows testing with a greater degree of realism than could reasonably be achieved with simulation scenario creation.
But until now, there was no way to understand the composition of the RF recording, so, as with the live signal environment, there was no way to know which elements in the environment produced what response in the DUT. That insight could only be gained by using controllable, synthetic signals generated by a GNSS simulator, like Keysight PNT X, GSS7000 or PNT Xe.
GNSS simulators are highly controllable and accurate, allowing precise testing which is critical for PNT device development. But no simulator can fully replicate the richness of a real-world environment. Field testing with live signals is therefore unavoidable—and often expensive, as it happens at a late point in the test cycle, making errors more costly to fix.
SimXTRACT: shortening test timescales by replicating real signals in the lab
Now, that’s all changing with SimXTRACT a new, software tool from Keysight.
SimXTRACT analyzes an RF recording and decomposes it into individual GNSS signals - including line-of-sight (LOS) signals and multipath reflections - and the key parameters of each. It then outputs the signals as fully-controllable drive data for use in a Keysight PNT simulator.
A controllable real-world signal environment means more field testing can be moved into the lab, from an earlier stage in the test cycle. Errors can be caught earlier, and test timescales can be shortened, accelerating time to market for new chipsets, devices or systems.
Key capabilities of SimXTRACT include:
- Signal decomposition and analysis: SimXTRACT uses a software-defined GNSS architecture with a patented signal searching algorithm to process and analyze IQ data recorded with a GSS6450. It separates Line-of-sight (LOS) and non-line-of-sight (NLOS) signals and decomposes each signal into a discrete ray path. For each satellite epoch, it provides key data, including:
- Number of rays (LOS + multipath)
- Code error of each ray
- Doppler error of each ray
- Power of each ray
- Angle of arrival (AoA) of each ray
SimXTRACT can also be used to search recordings for specific conditions, such as number of satellites in view, or number of multipath signals present.
- Scenario creation: SimXTRACT generates test scenarios for use with Keysight PNT X, GSS7000 and PNT Xe GNSS simulators. It turns the decomposed data into control files, which the simulator uses to generate the commensurate GNSS signals. All signals are fully editable and modifiable in the simulator, giving test teams full control over scenario parameters. For example, the power levels of multipath signals can be adjusted, or the signals can be disabled altogether.
- Spoofing detection and creation: SimXTRACT can distinguish between genuine GNSS signals and counterfeit signals produced by a spoofing device, which often exhibit behaviors not seen with genuine signals. If spoofing is captured in the recording, SimXTRACT provides an opportunity to analyze the signals and generate test scenarios based on genuine, real-world spoofing activity - an invaluable capability for characterizing receiver robustness and resilience. If spoofing isn’t present (as will usually be the case), it can be easily added to the scenario in the simulator.
SimXTRACT accelerates time to market across industries
SimXTRACT can benefit developers and integrators of GNSS receivers across many sectors. It enables the realism of the operating environment to be reflected in the lab, in turn enabling verification testing to ‘shift left’ in the product lifecycle - so that even software-based receiver designs can be tested with highly-realistic signals. Flaws and vulnerabilities can be identified far earlier, significantly reducing the cost, risk and timescales of product development, and improving the fitness-for-purpose of the product.
Some ways in which different industry sectors can benefit from SimXTRACT include:
- GNSS chipset development: Signal decomposition and analysis can accelerate the development of Measurement Engine (ME) and Position Engine (PE) algorithms for tasks such as signal acquisition and tracking and bit synchronisation. It can also help to determine the optimal cross-correlation margins for the different constellations, and to optimize navigation data decoding in different environments.
- Automotive: SimXTRACT enables the specific real-world effects seen in drive tests to take place much earlier in the development cycle. Decomposing and editing RF recordings in the lab enables the effects of multipath and signal obscuration at locations around the world to be much better understood than in the unquantifiable real-world signal environment. SimXTRACT can also be used to evaluate receiver performance in scenarios like deep urban and other highly obscured locations, as well as design decisions like antenna placement on the vehicle.
- Handsets and wearables: SimXTRACT can bring new efficiencies to over-the-air testing of multiple devices in an anechoic chamber. Its decomposition algorithm calculates the angle of arrival of each signal, allowing real-world effects to be reproduced very quickly in a zoned chamber setup without having to manually tune the simulator scenarios to produce them. It’s an effective way to test device performance with realistic multipath signatures. If spoofing is not present, it’s simple to add it on top of real-world recordings to enable testing against many different scenarios without the expense of repeating tests until they occur.
Talk to us about SimXTRACT today
SimXTRACT can significantly reduce the cost and timescales of verification testing, while greatly improving insight into PNT performance in real-world signal environments. To learn more read our latest eBook, Field Testing Moves into the Lab or contact us.