Positioning, Navigation and Timing testing software

Bridge the PNT Testing Gap: Bring Field Realism into the Lab

SimXTRACT tool analyzes and decomposes recordings of the live GNSS signal environment, providing unprecedented insight into multipath interference and other effects.

GNSS record and playback is a highly valuable tool for bringing real-world signals into the PNT test lab. But until now, developers could only use the recordings in limited ways.

The big benefit of record and playback is that a real signal environment can be played repeatedly to a device under test (DUT). This can help to characterize its real-world performance in a way that’s faster, more relevant, and more cost-effective than repeated field testing using live signals.

The problem is that the recording is one composite file, offering no insight into the signals and impediments present. If the DUT fails to perform as expected during playback, there’s no way of telling which (if any) characteristic of the signals in the recording caused the anomaly. It can only be investigated by trying to reconstruct the error state using a GNSS simulator, which can be a time-consuming process.

Keysight SimXTRACT extracts signals from live sky GNSS recordings

Keysight has addressed this issue with SimXTRACT: a patented software tool that extracts signals from a live sky recording, discretely quantifies them, and outputs them as drive files for use in a Keysight GNSS emulator.

SimXTRACT is set to transform GNSS testing, enabling more field-representative testing to be conducted in the lab, and to be conducted earlier in the test cycle.

For this blog, I’m going to dive into just one of SimXTRACT’s transformative capabilities: its ability to analyze and decompose recordings into individual signals.

How SimXTRACT works

SimXTRACT is designed for use with record & playback systems (RPS) such as the Keysight GSS6450, an ultra-portable unit which can record any RF signals in the 80 MHz to 6,000 MHz frequency range.

The GSS6450 takes high-resolution samples of the real-world signal environment, including its impurities and imperfections. Each recording is output as an I/Q file which can then be analyzed by SimXTRACT.

Analyze GNSS recordings and decompose IQ files into individual signals

Running on a GPU-equipped laptop or Keysight C50 X host controller, SimXTRACT employs a software-defined signal processing architecture with a patented signal searching algorithm. The algorithm analyzes the content of the I/Q file, decomposes each signal into a discrete ray path, and provides the following data for each satellite epoch:

The signal data extracted by SimXTRACT has two very powerful applications. The first is that it can be converted into drive files for use in a Keysight GNSS simulator. This means real-world signals can be replicated in simulation scenarios with full control over each signal—bridging the gap between field and lab, and revolutionizing test methodologies based on RF record & playback. The signals re-created in the simulator are over 95% real versus the signals captured in the field. Unprecedented realism!

Secondly, SimXTRACT includes analysis tools that allow users to search recordings for specific effects and behaviours. Search parameters are very granular—for example, searches can include criteria like number of satellites (SVs) in view, and the number of multipath signals present, and carrier-to-noise (C/No) ratios.

This allows developers to quickly home in on specific moments in a recording, rather than having to test over the entire duration of the recording. Decomposition also gives a truth measurement for the real world, which developers can use to check whether the receiver is finding all of the real-world errors, or is just being affected by them.

Overall, SimXTRACT’s signal decomposition and analysis capabilities represent a huge leap forward for record & playback test methodologies. Benefits for test teams are wide-ranging—from the ability to extract real-world signals for use in a simulator, to the ability to quickly locate and analyse specific conditions in the recorded environment.


Talk to us about SimXTRACT today

SimXTRACT can significantly reduce the cost and timescales of verification testing, while greatly improving insight into PNT performance in real-world signal environments. If you’d like to know more, please get in touch or download our eBook: PNT Field Testing Moves into the Lab.

limit
3