What the Best SBOM Solution Should Deliver

The Software Bill of Materials (SBOM) has become one of the most important tools in modern cybersecurity and software supply chain management. By listing the components that make up a piece of software or a device, SBOMs provide the visibility needed to assess vulnerabilities, ensure compliance, and maintain trust throughout the product lifecycle.

However, as SBOM adoption accelerates across industries, from industrial control systems to medical devices and telecommunications, many organizations are learning that not all SBOM solutions are created equal. Several widely used tools still struggle to meet the practical expectations and regulatory requirements emerging from frameworks such as the FDA guidance “Cybersecurity in Medical Devices: Quality System Considerations and Content of Premarket Submissions”, the EU Cyber Resilience Act (Regulation (EU) 2024/2847), PCI DSS v4.0, and CERT-In SBOM and extended BOM guidelines. Incomplete data, inconsistent formats, and overwhelming vulnerability lists have made it difficult for security teams to rely on SBOMs for actionable intelligence or for confident regulatory submissions.

To understand what the best SBOM solution should deliver, it’s important first to recognize that there are two distinct types of SBOM users, SBOM producers and SBOM consumers, each with unique needs and expectations.

SBOM Producers: Building Secure and Transparent Products

SBOM producers are manufacturers, software vendors, and device makers who generate SBOMs for the software and firmware they develop or integrate. Their primary objectives include:

For producers, the challenge lies in creating accurate, complete, and shareable SBOMs that truly represent what is shipped to customers, including third-party and open-source dependencies embedded deep within compiled binaries. Many still rely on limited, source-based tools that cannot detect components or vulnerabilities hidden in closed, proprietary, or native code, resulting in incomplete visibility and compliance gaps.

In addition, producers face increasing complexity in generating and maintaining VEX (Vulnerability Exploitability eXchange) documents, which communicate whether identified vulnerabilities actually affect a product and provide the vendor’s assessment and response regarding their exploitability. Creating accurate VEX data and keeping it synchronized with evolving SBOMs is often a manual, time-consuming process, especially when products have multiple versions or variants.

Producers must also manage secure and traceable distribution of both SBOM and VEX files to regulators, customers, and ecosystem partners making automation, consistency, and lifecycle management essential features of the best SBOM solutions.

SBOM Consumers: Understanding and Managing Software Risks

SBOM consumers are asset owners, operators, and enterprise security teams who receive SBOMs from their suppliers or extract them directly from deployed devices. Their objectives differ from those of producers but are equally critical to maintaining a secure and resilient environment.

Their priorities include:

For consumers, the biggest challenge remains trust. Trust that the SBOMs they receive are accurate, complete, and regularly updated. However, trust is only part of the problem. Most organizations also lack a centralized platform capable of ingesting, managing, and maintaining large volumes of SBOMs from multiple suppliers, in different formats, and across multiple product categories. Without such a system, SBOMs remain siloed and quickly lose value as software evolves. Another significant challenge lies in the lack of reliable mapping between SBOM data and the organization’s actual asset inventory. Many consumers struggle to align specific SBOMs with deployed hardware, firmware, or software versions, preventing effective vulnerability monitoring and remediation.

Bridging the Gaps: What the Best SBOM Solution Should Deliver

Despite growing demand and regulatory momentum, most SBOM tools today still fall short in six critical areas: accuracy and coverage, vulnerability management, secure sharing, CVE overload, overall quality, and consumer SBOM visibility. Let’s examine each of these challenges, and what the best SBOM solution should provide to overcome them.

1. Accuracy and Coverage

Achieving 100% SBOM accuracy across complex supply chains is a high expectation. Modern software and firmware often include hundreds of components, some compiled, some statically linked, some inherited through nested dependencies. These complexities make perfect accuracy nearly impossible, especially for closed-source or third-party code. However, the best SBOM solution should strive for significantly improved accuracy and coverage through smarter analysis and more advanced detection techniques. Many existing SBOM tools rely solely on build-time or source-level scanning, which leaves blind spots when examining the actual binaries shipped to customers. This means that what’s in the SBOM might not reflect what’s in the deployed product. The best SBOM solution should:

Keysight SBOM Manager achieves this with patent-pending binary SBOM detection technology that reveals deeply embedded components and improves accuracy and coverage for native code binaries. This approach gives both producers and consumers more confidence that the SBOM truly represents the software or device in use.

2. Vulnerability Correlation, Monitoring, and Context through Scalable VEX

Generating an SBOM is only the first step. Once released, software and firmware must be continuously monitored for newly disclosed vulnerabilities. However, many current SBOM tools fail to incorporate diverse and authoritative vulnerability intelligence sources, relying solely on the NVD (National Vulnerability Database) while overlooking vendor advisories, and other vulnerability and threat intelligence sources that provide crucial context. Without this broader perspective, organizations face incomplete or outdated risk assessments.

The best SBOM solution should:

Keysight SBOM Manager integrates multi-source vulnerability correlation, combining data from NVD, CISA KEV, OSVDB, Github security advisories, vendor advisories, and other sources to ensure accurate, up-to-date vulnerability intelligence. It continuously monitors SBOM components for new CVE disclosures and enables generation of VEX documents at scale, allowing security teams to easily incorporate exploitability context. By maintaining synchronization between SBOM and VEX data across versions, Keysight enables proactive and context-rich vulnerability management throughout the product lifecycle.

3. Scalable and Controlled SBOM Sharing

Regulations such as the EU Cyber Resilience Act and the FDA cybersecurity premarket guidance require manufacturers to maintain up-to-date SBOMs and make them available to regulators upon request as part of compliance and risk management obligations. While these regulations do not mandate sharing SBOMs directly with customers or partners, market demand is rapidly shifting in that direction. Increasingly, enterprise customers, integrators, and critical infrastructure operators require suppliers to provide SBOMs as part of their procurement and vendor assurance processes, often making SBOM transparency a precondition for purchase or continued partnership. Yet in practice, many organizations still share SBOMs manually through emails or file transfers, which are neither scalable nor secure. The best SBOM solution should:

This level of controlled, automated sharing transforms SBOMs from isolated compliance artifacts into living, shareable sources of product security truth.

Keysight SBOM Manager provides a centralized platform for secure and scalable SBOM distribution. Through role-based access control and built-in sharing workflows, producers can distribute SBOMs and VEX documents directly to customers, partners, and regulators without relying on manual file exchanges. Each shared SBOM is version-controlled and traceable, ensuring recipients always see the most recent and validated data. In addition, Keysight’s platform includes human-readable SBOM and VEX views, making it easier for non-technical stakeholders and regulators to review submissions with clarity and confidence.

4. Vulnerability Overload

A frequent frustration among SBOM users is vulnerability overload, when every potential vulnerability for every component is reported, regardless of relevance. While completeness sounds ideal in theory, in practice it overwhelms development and security teams, obscuring critical risks under a mountain of low-priority or irrelevant alerts. This issue is especially prevalent in SBOM tools that simply map every detected component to every associated CVE in the National Vulnerability Database (NVD) without any context. The best SBOM solution should:

While a few tools claim to perform vulnerability reachability analysis, their results are often inconclusive, the absence of a vulnerability marked as “reachable” does not necessarily mean it cannot be exploited. It simply indicates that the tools found no evidence suggesting reachability or exploitability. Fully automated exploitability detection remains beyond current technological capabilities.

Keysight SBOM Manager takes a more pragmatic approach by automatically filtering out many irrelevant vulnerabilities that are certainly not applicable and prioritizing the rest according to defined policies. This enables security teams to spend less time sorting through data and more time addressing real security risks.

5. Quality and Usability

Even a technically complete SBOM can be unusable if it contains inconsistent data, missing fields, or invalid relationships between components. Low-quality SBOMs cause import errors, break automated workflows, and lead to mistrust between suppliers and consumers, undermining the very purpose of software transparency. Quality in SBOMs is not just a best practice; it is increasingly a regulatory expectation. Frameworks and standards such as NTIA’s “Minimum Elements for a Software Bill of Materials (SBOM)” (2021), CISA’s “Minimum Elements for a Software Bill of Materials (SBOM) – 2025 Update”, the EU Cyber Resilience Act (Regulation (EU) 2024/2847), and regional initiatives like BSI Technical Guideline TR-03183-2: Software Bill of Materials (SBOM), and CERT-In’s Guidelines on SBOM, CBOM, QBOM, AIBOM, and HBOM (July 2025) define or reference minimum required fields that an SBOM must include to ensure interoperability and compliance. These fields typically cover critical attributes such as component name, version, supplier, unique identifier (CPE or PURL), dependency relationships, and other metadata. As these frameworks evolve, maintaining alignment with their requirements becomes essential for both product producers and consumers operating in regulated markets. The best SBOM solution should:

Keysight SBOM Manager incorporates advanced validation, correction, and normalization capabilities that ensure SBOMs meet the minimum required field expectations defined by CISA, BSI TR-03183, and CERT-In whenever possible. It automatically detects incomplete or inaccurate metadata, resolves naming or identifier inconsistencies, and enriches missing elements where derivable from binary or auxiliary data sources. By producing high-quality, standards-compliant, and regulator-ready SBOMs, Keysight SBOM Manager ensures that producers can confidently demonstrate compliance while consumers can integrate and analyze SBOMs reliably across their environments. For producers, this means consistent, submission-ready outputs across product lines. For consumers, it provides dependable, structured data they can act on confidently for vulnerability monitoring, procurement assurance, and compliance reporting.

6. Enabling Consumers to Integrate SBOMs for Full Asset Visibility

True lifecycle management extends beyond the producer’s side. SBOM consumers must be able to ingest, normalize, and map SBOMs (whether provided by suppliers or generated internally from binaries) to their actual deployed assets. Without this linkage, even the most accurate SBOMs fail to provide actionable visibility into operational risk. The best SBOM solution should:

Keysight SBOM Manager provides a unified consumer view, enabling organizations to ingest SBOMs from both suppliers and internal analyses. It automatically correlates SBOM data with deployed assets and device inventories to pinpoint where vulnerabilities actually reside. The platform continuously monitors SBOM components against live vulnerability feeds and integrates seamlessly with existing asset management systems. It also supports advanced, comprehensive search capabilities, for example, when a new CVE is disclosed, users can identify all affected assets with a single click and visualize the full impact across organizations and devices through an impact graph.

A Comprehensive Approach: Bridging the Gaps Across the SBOM Lifecycle

Each of these six pillars is essential but what sets the best SBOM solution apart is the ability to bring them together into one cohesive platform. Keysight SBOM Manager was purpose-built to unify these capabilities and serve both sides of the SBOM equation:

SBOM Generator provides deep binary analysis and accurate component identification.

SBOM Studio enables product producers to manage, validate, monitor, and share SBOMs and vulnerabilities through the entire lifecycle.

SBOM Consumer empowers users and asset owners to ingest supplier SBOMs, assess vulnerabilities, and track ongoing risks.

This ecosystem bridges the traditional gap between producers and consumers by transforming SBOMs from static compliance artifacts into living security assets.

Conclusion: From Compliance to Confidence

The global push for software supply chain transparency is reshaping how organizations manage product security. Yet, visibility alone is not enough. The real challenge lies in trusting that visibility, trusting that your SBOM data is accurate, complete, and actionable. The best SBOM solution is not the one that generates the most data, but the one that delivers the most reliable and actionable insight. It must address every stage of the SBOM lifecycle and the needs of both producers and consumers by excelling in the following six pillars:

With Keysight SBOM Manager, organizations can achieve this balance by bridging the gaps in SBOM accuracy, quality, and usability to move beyond compliance and build true supply chain confidence.

limit
3