digital finger print on computing board

From Sensor to Server: Securing Biometric Authentication Solutions

Biometric authentication is now part of critical user journeys: unlocking devices, authorizing payments, and accessing private information. Adoption is strong because the experience is fast and familiar, yet it expands the places where things can go wrong. The right question is not only whether your system works for honest users. It is how it fails under pressure, and which adversaries you need to resist.

Keysight’s Biometric Security Evaluation addresses that need with end-to-end assurance. We examine the full chain—from sensor to model, from operating system to application, and from client to backend. The goal is to produce evidence you can use, whether in meeting compliance requirements or developer security standards. We combine architectural review with hands-on testing and translate results into practical steps that strengthen the system without harming user experience.

Threats to Biometric Authentication

Biometric systems face threats at multiple layers of the pipeline:

1. Sensor-level attacks
Many attacks begin at the sensor. Presentation attacks (spoofing) use printed faces, 3-D masks, or artificial fingerprints to bypass weak liveness checks.

2. Data injection and replay
If defenses focus only on the sensor, attackers shift downstream. They may inject or replay synthetic frames, manipulated feature vectors, or forged “match” signals after capture.

3. Runtime compromise
Rooted or emulated devices can hook APIs, substitute or simulate sensors, and trigger permissive fallback paths.

4. Device–server trust
Trust can also fail at the boundary. If a backend accepts unverified claims about secure boot, device state, or TEE integrity, a strong model still produces weak assurance.

5. Template handling
The way biometric templates are stored and managed matters. Weak access controls, poor storage, or improper lifecycle handling amplify compromise impact and raise privacy risk.

None of these weaknesses exist in isolation. A single weak link can undermine otherwise solid defenses, which is why our evaluations assess the system as a whole.

Understanding Adversaries

Threat modeling only works when aligned with real adversaries:

We tailor each assessment to the capability tier that matches your exposure. This ensures test pressure reflects the real-world environment your product must withstand.

This service is aimed at teams that need measured assurance, not assumptions. Product owners want fewer surprises two sprints before launch. Security architects want data that supports design decisions. Program leads need clarity before partner reviews. OEMs and integrators must confirm that third-party SDKs behave as expected across OS, TEE, and application boundaries. In each case, the outcome should be the same: a defensible picture of risk and a roadmap that your engineers can deliver.

Tailored Services for your Unique Architecture and Development Stage

1. Threat Modeling
Our engagement typically begins with threat modeling. Together, we:

2. Security Design Review
We then analyze the system design end to end:

3. Hands-on Testing
Next, we validate resilience through practical testing:

All steps are fully documented to ensure reproducibility. Your team can replicate results, speeding resolution and reducing debate.

4. Analysis and Recommendations
We transform findings into actionable guidance, prioritized by impact and ease of exploitation:

A targeted retest confirms fixes close the intended gaps and helps identify regressions.

5. Clear Deliverables
We provide outputs tailored to different stakeholders:

Security Testing for Compliance and Assurance

Backed by industry accreditations across major compliance schemes, including programs such as EMVCo, Mastercard CAST, and Microsoft SDCP, we can align your security testing work with the standards your partners expect. Whether you need to meet formal compliance requirements, integrate a new biometric feature, or harden your solution, we can tailor our evaluation depth and deliverables to fit your unique product. That means scoping to your architecture, risk profile, and market goals; coordinating with your internal teams and vendors; and balancing security gains with UX, performance, and cost.

Compliance matters, but it should not lead the security conversation. Programs such as EMVCo, CAST, or SDCP are important for market access and partner trust, but they are also easier when your fundamentals are sound. Building strong attestation, secure template lifecycle, and trustworthy decision flows first turns certification into validation rather than discovery. So that by the time you engage in formal evaluations, you already understand the state of your security condition.

To learn more about Keysight’s Biometric Security Evaluation Service, visit our webpage, or reach out to our team today at [email protected].

Related Posts

limit
3