Quantum Computer

Understanding Post-Quantum Cryptography Standards & Compliance

The transition to post-quantum cryptography (PQC) is no longer a matter of “if,” but “when.” With the standardization of PQC algorithms now underway and compliance expectations clearly forming across global jurisdictions, organizations must begin preparing their products and systems today to ensure long-term security, interoperability, and market access.

Government agencies, regulators, and international standards bodies are publishing concrete requirements for the integration of quantum-safe algorithms. These standards will shape future cryptographic design and validation practices, especially for sectors such as automotive, telecom, healthcare, and defense. In this blog post, we explore the most important developments in PQC standardization and what security and business teams need to do now to stay ahead.

The State of PQC Standardization

After a six-year evaluation process, the U.S. National Institute of Standards and Technology (NIST) finalized its first set of PQC algorithm recommendations. These algorithms are designed to replace RSA and ECC in environments where long-term confidentiality and resistance to quantum attacks are essential.

The first set of selected algorithms includes:

These algorithms are being incorporated into FIPS 140-3 validation paths for cryptographic modules used in government and enterprise systems.

Internationally, ISO/IEC is aligning with these recommendations through updates to standards such as ISO/IEC 14888 (digital signatures) and 18033 (encryption schemes). ISO has also standardized XMSS and LMS, stateful hash-based signature schemes, since 2018–2020.

These developments mark a shift from theoretical discussion to practical implementation. The message is clear: the standards are here. The window to prepare is now.

Regulatory Expectations Are Taking Shape

Multiple government agencies and regulatory bodies are issuing guidance that mandates or encourages PQC adoption within defined timelines. These include:

These requirements signal a coordinated international effort to modernize cryptographic defenses in preparation for quantum threats—and compliance will increasingly become a gating factor for product approvals and government procurement.

Business Risk and the Cost of Inaction

While PQC is a technical transition, the implications are strategic. Delaying migration can introduce several business risks:

Cryptographic infrastructure is foundational. Strategic decisions made today will determine whether systems remain secure and compliant in the coming decade.

Secure Implementation Starts with Architecture

Even when quantum-safe algorithms are correctly selected, poor integration can still expose systems to attacks. PQC algorithms are larger and more complex than their classical counterparts, making them more challenging to implement securely—especially in constrained environments like IoT devices, smartcards, and embedded firmware.

To support long-term security and compliance, product teams should prioritize:

How Keysight Helps Organizations Prepare

Keysight supports product developers and security teams in aligning with emerging PQC standards and compliance frameworks. Our solutions span:

From firmware to secure elements, Keysight provides the expertise and tools to help organizations build and certify quantum-ready systems.

PQC adoption is no longer optional for organizations building secure products with long-term data protection requirements. Standards have been finalized, regulators are publishing timelines, and the cryptographic transition is actively underway.

To remain secure and competitive, businesses must move now to:

Secure implementation is not just a technical checkbox—it’s a business imperative.

Keysight helps teams navigate this transition with testing solutions, compliance expertise, and practical guidance on integrating PQC securely. For more information, reach out to us at [email protected].

Related Posts

limit
3