Prompt Injection Techniques: Jailbreaking Large Language Models via FlipAttack

A prompt is the input or instruction given to a large language model (LLM) to generate a desired response. Prompt injection is a security vulnerability where malicious input is crafted to manipulate the behaviour of a large language model (LLM), often causing it to generate unethical or inappropriate responses that override the original intent of the prompt.

Prompt injection has grown as LLMs are integrated into apps and workflows. According to recent findings, major AI applications tested showed vulnerability to prompt injection, for example refer to this attack. OWASP recognized the growing threat and listed Prompt Injection as the #1 risk in its 2025 OWASP Top 10 for LLM Applications.

There are two types of prompt injection direct and indirect, in this blog we are going discuss about a direct prompt injection through FlipAttack and discuss about its support in BreakingPoint Systems (BPS) and CyPerf.

FlipAttack Based prompt injection

Recently, the security researchers from ATI Keysight came across a research paper that introduces a clever and impactful prompt injection technique known as FlipAttack. This method has four different flipping variations in which it alters the characters order in prompt messages and achieves an 81% average success rate in black box testing, ∼98% attack success rate on GPT-4o and ∼98% bypass rate against 5 guardrail models on average.

Key Attack Vectors:

1.Prompt Disguise:

In this attack the malicious prompt is disguised using 3 different variants:

Figure 1: Python code for flip functions

2. Flipping Guidance:

This module is designed to guide LLMs in interpreting disguised prompts by employing a flipping task, ultimately enabling the models to recognize and carry out the underlying harmful intent.

The finely crafted prompt contains both the prompt disguise and flipping guidance which together trigger a prompt injection attack jailbreaking the LLM into generating unethical, attacker-desired responses.

Figure 2: Attack flow (source of the image ARXIV)

Leveraging FlipAttack Techniques to Jailbreak LLM Models

We tested the FlipAttack-based prompt injection on OpenAI's GPT-4o, GPT-3.5-turbo, grok-2-latest and gemini-2.0-flash models and found that all of the models were tricked by these methods, responding to prompts it would usually block. This showed a clear weakness in how it handles unusual input formats.

Figure 3: Sample FlipAttack-Based Prompt Injection Attack Response of GPT-4.0

FlipAttack Based Prompt Injection Strikes in BPS

At Keysight Technologies, our Application and Threat Intelligence (ATI) team added the support of this new type of Prompt Injection attack i.e. FlipAttack-Based prompt injection in ATI-2025-08 StrikePack.

This update includes three new strikes named “flipattack_fcs,fcw,fwo” which uses FlipAttack based prompts to jailbreak LLM's. These strikes will randomly select a jailbreak prompt and uses during the attack simulation.

Figure 4: List of FlipAttack based prompt injection Strikes

FlipAttack Based Prompt Injection Strikes in CyPerf

In an upcoming update CyPerf will add a set of strikes simulating Flip Attack Prompt Injections, which includes 3 variants of strikes designed to test three different LLMs: Grok, Gemini and OpenAI ChatGPT. Each of these 3 LLMs can be targeted by 3 different FlipAttack Strike Variants: Flip Characters in Word (FCW), Flip Complete Sentence (FCS), and Flip Words Order (FWO).

These prompts typically contain some instructions within the system prompt wherein the LLM is commanded to not repeat the user prompt (the actual malicious request) and to also not generate any response which has contrary intentions. These instructions are then followed by an unscrambling instruction where the LLM is made aware as to how it can obtain the actual request prompt from the given user prompt which is presently jumbled in any of the 3 formats.

The user prompt contains a single line where we supply the actual malicious prompt in a jumbled manner so that it does not trigger the LLM guardrails and gets executed stealthily.

In the CyPerf UI, this strike is available in both the Attack library and the Custom Attack sections, allowing users to easily select and run it as part of their test scenarios.

Figure 5: CyPerf UI displaying all available FlipAttack-based strike configurations

These strikes have configurable settings like choosing the target LLM's model (for example: gemini-1.5-pro) and changing the API version and key. These options allow for customization of strikes to match specific test traffic requirements.

A screenshot of a computer AI-generated content may be incorrect. Figure 6: Configurations exposed by Strikes and Actions panel

The statistic view in Cyperf UI provides detailed statistics from the test run, including the number of connections made and the number of active client and server agents. It can be seen if the strike and/or response were allowed to pass through the DUT. If the request successfully reaches the server, then the Server Allowed field shows an increment. If the response from the Server is allowed to pass through as well, then the Client Allowed field shows an increment.

Figure Figure 7: Run-time stats view in CyPerf UI

Figure 8: Strike statistics view in CyPerf UI

FlipaAttack-based prompt injection shows a smart and creative way to test how secure large language models really are. As more companies start using AI systems, it's important to find and fix weaknesses to keep these technologies safe, trustworthy, and to make sure AI tools are used in a secure and responsible way.

Leverage Subscription Service to Stay Ahead of Attacks

Keysight's Application and Threat Intelligence subscription provides daily malware and bi-weekly updates of the latest application protocols and vulnerabilities for use with Keysight test platforms. The ATI Research Centre continuously monitors threats as they appear in the wild. BreakingPoint and in the future, other tools like CyPerf, now provide customers with access to attack campaigns for different advanced persistent threats, enabling them to test their currently deployed security controls' ability to detect or block such attacks.

References

  1. https://arxiv.org/pdf/2410.02832
  2. https://github.com/yueliu1999/FlipAttack
  3. https://genai.owasp.org/llm-top-10/
limit
3