A screen shot of a city Description automatically generated

Understanding Plex UDP Amplification DDoS Attack

In the era of online streaming media, Plex Media Server is a popular versatile software application that allows its users to organize, stream and manage their personal media contents (movies, TV shows, music and photos) across multiple devices. It’s like someone’s own Netflix server which can be accessed from their personal devices like smartphones, tablets, smart tv or any other streaming devices.

However, its popularity and widespread use also make it a popular target for an attacker. One significant vulnerability, which impacts the Plex Media Server is UDP Amplification DDoS attack discovered in 2021. One CVE-2021-33959 is also assigned to this specific vulnerability.

In this blog we will take a closer look at the traffic pattern of this attack including how one can reproduce the vulnerable setup and its exploitation.

Vulnerable Setup and Exploitation

As per the information provided by MITRE, Plex Server 1.21 and below is vulnerable to the DDoS Reflection attack. So, to understand the vulnerability better, ATI team has deployed a vulnerable environment locally using the Plex Media Server of version 1.9.5.3112 (victim) as shown below –

Inserting image...

Figure 1: Vulnerable Plex Media Server running on localhost

For the exploitation, we as an attacker are sending the payload “M-SEARCH * HTTP/1.1” to the vulnerable Plex Media Server on UDP port 32414 using the following ‘netcat’ Linux command –

echo “M-SEARCH * HTTP/1.1” | nc -u <server_ip> 32414

This triggers a UDP response from the server which is significantly larger than the original request as shown below -

Inserting image... Figure 2: Payload sent by the attacker and Exploitation

Interestingly, we have also observed that it is not just that exact “M-SEARCH * HTTP/1.1” payload. An attacker can send any successive substring of the same payload starting from the beginning (as shown below) in byte string format such as “\x4d” (“M”), “\x4d\x2d” (“M-”) and so on to the same UDP port 32414, the server still responds.

Inserting image... Figure 3: List of exploitable payloads

This indicates that the server starts processing and responding to the incomplete/partial UDP request as shown below –

Inserting image... Figure 4: Exploitation results for different vulnerable payloads

For this UDP Amplification attack the maximum Bandwidth Amplification Factor (BAF) we are getting is -

Inserting image...

Figure 5: Calculation of BAF

Attack Traffic Analysis

From the captured network traffic we can see that the vulnerable Plex Media Server is responding with a HTTP 200 OK response inside the UDP stream as shown below –

Figure 6: Sample traffic capture of the attack

This response contains the following headers –

Plex UDP Amplification DDoS Attack Traffic in Keysight ATI

At Keysight Technologies, our Application and Threat Intelligence (ATI) team, researchers have examined the traffic pattern of Plex UDP Amplification DDoS attack and its related strike (CVE-2021-33959) and added their support as part of BreakingPoint System’s DDoS Lab and Security component in ATI-2024-24 StrikePack released on December 06, 2024, as shown below -

Figure 7: Plex UDP Amplification DDoS Attack in BreakingPoint DDoS Lab

Figure 8: Plex Media Server Simple Service Discover in Response Strike in BreakingPoint

Leverage Subscription Service to Stay Ahead of Attacks

Keysight's Application and Threat Intelligence subscription provides daily malware and bi-weekly updates of the latest application protocols and vulnerabilities for use with Keysight test platforms. The ATI Research Centre continuously monitors threats as they appear in the wild. Customers of BreakingPoint now have access to attack campaigns for different advanced persistent threats, allowing BreakingPoint Customers to test their currently deployed security control's ability to detect or block such attacks.

limit
3