Security Highlight: How Hackers Obtain Remote-Code-Execution in WhatsApp
CENSUS Labs has recently identified several Man-in-the-Disk vulnerabilities in the popular Android application WhatsApp. The cybersecurity engineering company reported that an attacker can chain these vulnerabilities to execute arbitrary code on a victim device. We find these vulnerabilities extremely interesting as it involves a complex interaction of various components from various vendors, which ultimately breaks assumptions regarding trust boundaries. But first, let’s look at the stages of the exploitation process that an attacker executes. The process begins by exploiting a vulnerability in the Chrome browser to bypass the Same-Origin-Policy for local content. The attack involves tricking the victim into opening a specially crafted HTML document in Chrome, enabling exfiltration of specific local files from the internal storage of an Android device.
The next step of the attacker’s exploitation process is to exfiltrate files containing Transport Layer Security (TLS) cryptographic material used to secure the communication between the WhatsApp client and backend servers. The vulnerability here is that WhatsApp stores TLS session keys as files in the internal storage of the device that is accessible by other applications or components. Therefore, this storage is not fully private to the WhatsApp application itself.
Once these cryptographic keys are exfiltrated, an attacker can perform a Man-in-the-Middle attack and decrypt or modify the communication between WhatsApp and the backend servers. This part of the attack requires the capability of re-routing network traffic to pass through an attacker-controlled node. Even though this part of the attack is left out of scope in the article, it is still realistic, depending on the scenario and network topology, for victim traffic to be re-routed.
Having Man-in-the-Middle capabilities, an attacker then modifies a ZIP archive downloaded by the WhatsApp application in-flight containing doodles and various emojis. The modified ZIP file takes advantage of two other vulnerabilities in the WhatsApp application, allowing an attacker to overwrite files on the device containing code executed by WhatsApp. That arbitrary code is executed with the privileges of the WhatsApp application itself, thus enabling an attacker to alter its behavior completely or access message contents.
Besides the complex interaction of components, notice that no memory corruption vulnerability is exploited in this attack. The full chain is built upon individual vulnerabilities that expose private artifacts (cryptographic keys, code) to an attacker. Addressing such issues requires a good understanding of how the various components of a system interact with one another. This exercise is far from trivial, requiring combined knowledge of both the Android platform, threat modeling, security architecture, and code reviews.
If you have any questions, contact us at [email protected].