PCB Design Software | Schematic Graph Illustration

Go From Idea to Launch With RF PCB Design Software


Key takeaways:

Complex RF PCBs are at the heart of many modern critical devices, like radar transceivers, telecom base stations, and wireless routers. Designing RF PCBs is a complicated task requiring years of experience and proficiency because every little change can have severe ripple effects on functionality and performance.

RF PCB design software assists in engineering these sensitive boards with high confidence and productivity. Learn why this software is essential to RF design and what features to look for when evaluating them.

What is RF PCB design software?

RF PCB design software is a specialized category of electronic design automation (EDA) tools for designing, simulating, and verifying PCBs that operate at high frequencies in the following bands:

At these high frequencies, several physical phenomena that are otherwise negligible show prominent effects on a PCB's functionality and performance. They include transmission line effects and electromagnetic interference (EMI) from copper traces, propagation losses in the PCB layers, parasitic effects of inductors and capacitors, higher resistances due to skin effects, noise, phase shifts, and more.

Even minor changes to an RF circuit board design — like slightly increasing the dimensions of traces — can intensify these effects and severely impact functionality or performance. RF PCB design is a delicate balancing act that, when done manually, can severely hamper design productivity.

This is where RF PCB design software helps, ensuring high first-pass yield and faster time-to-market. It provides sophisticated circuit simulation and analysis models to see the impacts of the above phenomena after every change in the PCB layout or schematic. It automates the optimization of RF board layouts and routing using in-depth knowledge of RF phenomena.

Let's dig deeper into why RF PCB design tools are practically a necessity nowadays.

Why is RF PCB design software essential for creating wireless electronic circuits?

Pcb Design Software | Rf Pcb Design Software Essential for Creating Wireless Electronic Circuits | Essential Circuit Parts

Figure 1. High-frequency effects

The delicateness of RF PCBs calls for precise control over all design aspects and high-frequency phenomena. Even minor changes must be carefully evaluated for potential ripple effects on the PCB's functionality and performance. We outline some of these phenomena, aspects, and effects in more detail below.

High-frequency (HF) phenomena

Frequency is, by far, the most important factor because of its first-order and higher-order effects. These must be simulated and mitigated using RF PCB design software.

Since the wavelengths of HF signals are comparable to the dimensions of components and circuit traces, effects like resonance and standing waves occur. They must be mitigated through precise control over trace geometries and floor layouts.

Electromagnetic effects become pronounced. Copper traces start behaving like transmissionlines instead of simple wires. Signals experience reflections, delays, and attenuation due to impedance mismatches. Engineers must account for factors like transmission line lengths relative to the typical signal wavelengths.

Another problem is increased resistance due to the skin effect — the tendency of HF alternating currents to concentrate near conductor surfaces instead of flowing evenly through the entire cross-section.

Then there are the parasitic effects. Every inductor is also a capacitor, and every capacitor is an inductor. They cause unexpected resonant frequencies and phase shifts. All analyses and simulations must use their equivalent circuits for accurate results.

Nonlinearities in active components like diodes and transistors become more pronounced. Their unexpected harmonics and intermodulationnoise can degrade desired signals.

Signal integrity issues

Signal integrity covers concerns like:

Techniques like controlled impedance, differential signaling, and ground planes are necessary to maintain signal integrity. RF PCB design environments integrate all these analyses into user-friendly workflows to enable quick checks and visualizations.

Power integrity concerns

Power integrity concerns include:

Thermal effects

Heat dissipation and thermal management are essential to prevent effects on signal integrity. Substrate materials with lower coefficients of thermal expansion (CTE) and loss tangents are essential. Design software must be able to model and predict the thermal behaviors of these materials and their layer stack-ups. They must also predict the impacts of thermal behaviors on electrical and RF performance.

Materials and substrate concerns

Selecting the right materials for the various layers—conductive, substrate, surface finish, solder mask, and silkscreen—is crucial for RF PCBs. Substrate materials' dielectric constants (Dk), conductivity, permeability, and loss tangents affect propagation losses and noise.

Instead of common PCB materials like flame-retardant woven glass-reinforced epoxy resin (FR4), RF PCBs prefer polytetrafluoroethylene (PTFE) because its dielectric properties and lower loss tangent results in less HF signal attenuation.

PCB design software must support the modeling of all these aspects and facilitate dielectric constant matching for various stack-ups.

Layout and routing impacts

Mitigation of many HF phenomena involves careful design of layouts, routing, and geometries. These aspects include:

These layout aspects are like a web — a minor change in one region can have ripple effects on everything else. So automatic checks and adjustments are essential for productivity.

What are the main features to look for in RF PCB design software?

Features to Look for in Rf Pcb Design Software | Thermal Analysis, Rf Circuit Synthesis | Essential Capabilities of Rf Pcb Design Software

Figure 2. Essential capabilities of RF PCB design software

How do you choose the best PCB design software for your wireless project needs? We outline the key features you should look for to streamline your RF PCB design workflows.

RF circuit synthesis features

Circuit synthesis capabilities must include the following:

Schematic capture capabilities

Look for the schematic design features listed below:

Layout and routing features

Some essential layout and routing features are outlined below:

Signal integrity and simulation capabilities

Real-world modeling and simulation features like the ones below are crucial for good RF PCB designs:

Fabrication output features

RF design software must generate the output formats required for PCB manufacturing. They include Gerber, Open Database (ODB++), and the Institute of Printed Circuits (IPC) standards like IPC-2581 for communicating design information to PCB manufacturers and IPC-D-356A for describing netlists.

What are the differences between RF and regular PCB design software?

Some key differences in functionality between regular and RF PCB software are listed below:

What are the best practices for designing multi-layer wireless PCBs using RF PCB design software?

RF PCBs use more layers than regular PCBs. Multiple layers enable designs to isolate sensitive signal paths, reduce crosstalk, control impedance, reduce EMI from power and ground planes, and mitigate thermal effects.

Key best practices for their designs are outlined below.

Layer stack-up design

Optimize layer arrangement using the following guidelines:

Layout and routing

Follow these guidelines:

Material selection

Select materials for the substrate and other layers according to the following recommendations:

Simulation, DRC, and testing

Place test points carefully to avoid interference with RF paths.

SPICE models and other RF models are available. Use them along with advanced electromagnetic simulation tools to thoroughly analyze signal integrity and RF performance after every change. This includes reflection analysis, crosstalk analyses, pre-layout simulations, and post-layout simulations.

Use specialized PCB design tools with comprehensive RF-specific DRCs and net-by-net analysis capabilities to ensure layout integrity and standards compliance.

How does Keysight's RF PCB design software facilitate wireless projects?

Keysight’s Rf Pcb Design Software | Keysight Ads

Figure 3. Keysight ADS

The Keysight Advanced Design System (ADS), a key part of the circuit design suite, is the leading solution for RF and microwave PCB schematic capture, layout, and simulations. It provides an easy-to-use design environment and promotes best practices through integrated design guides.

ADS provides a seamlessly integrated, all-in-one environment for conducting interactive signal integrity analysis, power integrity analysis, circuit simulations, electro-thermal co-simulations, and 3DEM simulations.

For accurate signal integrity analyses, ADS includes linear circuit, nonlinear harmonic balance, and circuit envelope simulations. It can run SPICE simulations of RF components like amplifiers. It implements EM simulation techniques like momentum and finite element methods to predict signal integrity challenges in high-speed designs. Powerful statistical tools can identify issues during design and improve manufacturing yield. It can generate X-parameters through accurate nonlinear modeling for HF designs.

ADS integrates digital signal processing capabilities with RF simulations for accurate mixed-signal co-simulations.

ADS includes advanced DRCs and layout vs. schematic (LVS) tools to identify RF bottlenecks and mistakes after each change.

ADS includes extensive RF component libraries and process development kits from leading foundries, ensuring a seamless transition from design to production.

Create flawless RF PCB designs with Keysight

Rf Pcb Designs With Keysight | Flow of Keysight Rf Circuit Design Tools

Figure 4. Keysight RF circuit design tools

In this article, you obtained an understanding of the features necessary in RF PCB design software like Keysight's ADS.

To go deeper, enroll in the RF Board Design Flow Educational Bootcamp.

limit
3