Modern Satellite Communications (Satcom) | Different Orbital Altitudes and Velocities

Inside the Magic of Modern Satellite Communications


Key takeaways:

While you're reading this, some 6,000+ satellites are giving homes and offices around the world access to broadband Internet. More than 100 satellites are helping people everywhere navigate their roads, and perhaps thousands of satellites are ensuring our national security. For all these capabilities, you can thank the magic of satellite communications.

This blog post introduces you to the workings of satellite communications for telecommunications, broadcasting, internet connectivity, and defense uses. Get to know how key satellite characteristics are determined for a use case, and learn about the latest advances in satellite technology.

What are satellite communications?

SATCOM involves the use of satellites to wirelessly relay signals between transmitters and receivers on the ground when terrestrial wireless signaling between them is impractical due to their locations or the distances between them.

Satellite communications are used for:

Most of these communications systems are also relevant to other fields, like remote sensing and global positioning that use satellites. However, they use satellites as sensors that measure something rather than mere relays.

How do satellite communications work?

The orbits of communications satellites can range from 160-36,000 kilometers (km), or 100-22,400 miles. To communicate wirelessly over such distances, satellite communications have to rely on electromagnetic (EM) waves.

The Earth's atmosphere and ionosphere are opaque to most EM frequencies, except for some bands in the radio, microwave, visible light, and infrared frequencies.

Our focus will be on satellite communications using radio frequency (RF), microwave, and infrared signals.

Every satellite communication system has a space segment and a ground segment.

The space segment consists of all the satellite or satellite constellations as well as the ground station control systems responsible for tracking, telemetry, control, and monitoring (TT&C, or TTC&M).

The ground segment consists of the ground stations or terminals that transmit data to or receive data from the satellites and their interconnections over terrestrial wired or wireless networks.

The wireless link from a terminal or ground station going toward a satellite is called an uplink. A link going from a satellite toward a terminal (or ground station), in turn, is called a downlink. An end-to-end link between two terminals via one or more satellites is a channel. Data flow in a link may be one-way for some use cases (like broadcasting) or two-way (like internet connectivity). However, TT&C communication is always two-way.

What are the different types of satellites used for communication?

The satellites used in these fields are categorized based on their orbits, use cases, or functions.

Orbital parameters like altitude, inclination, and velocity are crucial in the design of satellite communications. Orbital altitudes can range from 160-36,000 kilometers. The lower the height, the faster the satellite has to orbit around the Earth to counteract its gravitational pull. Simultaneously, due to its rotation, each point on the Earth's surface moves underneath a satellite by some kilometer every minute (27 km at the equator). All these aspects have to be accounted for while establishing uplinks and downlinks.

Altitude is the most important parameter. Based on it, there are the following types of satellites:

A satellite orbit is chosen based on its use case and function. Each orbit has pros and cons. For example:

How do radio satellite communications work?

RF and microwave frequencies are the most common bands currently used in satellite communications. These frequencies are divided into a number of bands with different designations as shown below

Satellite Communications | Rf and Microwave Frequency Bands Graph | Satellite Communications

Figure 1. RF and microwave frequency bands (not to scale)

What is the role of frequency bands in satellite communications?

The bands are chosen based on the use case. For example:

Importantly, the uplink and downlink frequencies are always different but operate within the same band. If they're the same, the uplink filter of a satellite can't differentiate between legitimate input signals from a ground station and feedback from its own downlink antenna.

What is the RF architecture of a satellite?

Satellite Communications | Rf Block Diagram of a Relay Satellite | Architecture of a Satellite

Figure 2. RF block diagram of a relay satellite

Ground stations and mobile satellite terminals transmit radio signals to satellites using quadrature amplitude modulation (QAM). These signals are received by the satellite and are either decoded or relayed.

The communications payload of a relay satellite consists of a transponder and antennas as shown above. It consists of these main components:

For decoding TT&C commands and received data, the following additional components are required:

For transmitting data, the following components are required:

How does optical satellite communication work?

Some modern satellite constellations use inter-satellite optical links to communicate with each other. These use infrared lasers to carry commands and data. High bandwidths and lower susceptibility to interference are some of their benefits.

What are the primary applications of satellite communication in various industries?

Satellite communications are used in multiple industries:

What are some technological advances in satellite communications?

Some recent developments and advances in satellite communications include the following:

Keysight empowers your satellite communications

This blog post outlined the major concepts and subsystems that make up satellite communications and gave an overview of recent advances in the field.

Keysight has an extensive portfolio of test and measurement products and software to cater to every subsystem of your satellite communication systems and provide satellite mission assurance.

Contact us for expert insights and recommendations on optimizing your satellite communications.

limit
3