A Comprehensive Guide to Installing BenchVue Basic
Welcome to the comprehensive guide for installing BenchVue Basic, a powerful software tool that unlocks the full potential of your instruments. In this blog post, we'll not only explore what BenchVue Basic is but also provide you with a step-by-step installation guide to simplify the process.
What is BenchVue Basic?
BenchVue Basic is a free version of software from the PathWave BenchVue software family. It's designed to simplify and enhance your test and measurement tasks by providing an efficient platform for controlling and automating your instruments.
The Transition: From BenchVue Included License to BenchVue Basic App
One of the most significant recent developments is the transition from the BenchVue Included License to the BenchVue Basic App. This transition simplifies the user experience by eliminating the need for a separate license and complex installation processes, making access to the powerful PathWave BenchVue software more convenient.
Key Changes:
- License Activation: With the BenchVue Basic App, you no longer require a BenchVue Included license, starting with platform version 2022.1. The activation process has been eliminated, allowing you to use the BenchVue Basic Apps immediately.
- Technical Support: It's important to note that BenchVue Basic Apps do not come with technical support. If you require assistance or access to the latest software version, we recommend opting for the licensed version of the app.
Why BenchVue Basic?
Here are four compelling reasons to choose BenchVue Basic:
- Effortless Access: BenchVue Basic simplifies the process of license redemption and installation. You can start using it right away.
- Seamless Integration: BenchVue Basic effortlessly integrates your instruments into your workflow, making it easy to control, automate, and monitor them. This saves you valuable time and effort.
- No Limitations: BenchVue Basic offers unlimited access to a wide array of features and capabilities. Whether you need to perform measurements, analyze data, or automate tests, BenchVue Basic has you covered without restrictions.
- Cost-Efficiency: BenchVue Basic is free, making it a cost-effective solution for professionals who want to harness the full power of PathWave BenchVue without incurring additional expenses.
Getting Started with BenchVue Basic
Starting your journey with BenchVue Basic is straightforward. You can find the software at www.keysight.com/find/BVBasic. BenchVue Basic offers both online and offline installers, allowing you to choose the one that best suits your needs.
Online Installer: We recommend the online installer when possible. It's smaller, downloads faster, and ensures you have access to the latest features, bug fixes, and security patches.
Offline Installer: The offline installer is designed for situations where an internet connection isn't available. While larger, it's a suitable alternative when online installation isn't feasible.
System Requirements:
Before installation, ensure that you:
- Uninstall any existing BenchVue apps on your PC.
- Install the .NET Framework 3.5. Detailed installation guidelines can be found here.
Step-by-Step Installation Guidance:
For the online installer:
- Visit www.keysight.com/find/BVBasic.
- Scroll down to the "BenchVue Basic Online Installer" section.
- Select the BenchVue app you need and click the provided download link.
For the offline installer:
- Visit www.keysight.com/find/BVBasic.
- Scroll down to the "BenchVue Basic Offline Installer" section.
- Download the offline installer ZIP file.
- Save the ZIP file to your hard drive.
- Locate the downloaded ZIP file, right-click it, and select "Extract All." Follow the on-screen instructions to extract the files, which will be placed in the same directory as the ZIP file.
- Navigate to the directory where the extracted files are located, then double-click on the installer to commence the software installation.
- For detailed installation guidance, refer to the ReadMe file named "ReadMe_First.txt" included with the download.
Supported Instruments by BenchVue Basic Apps
A comprehensive list of supported instruments ensures you have the right tools at your disposal. Check out the list here.
Summary
The transition from the BenchVue Included License to the BenchVue Basic App is a game-changer in simplifying the user experience. It enables you to fully harness the power of the PathWave BenchVue software without the complexities of additional licenses and installations. Whether you're in a research lab, a manufacturing facility, or an educational institution, BenchVue Basic makes it easier to connect to your instruments and collect crucial data.
However, it's important to note that while BenchVue Basic is an excellent starting point, it doesn't offer the latest features, enhancements, or technical support that the licensed BenchVue app provides. To access these advanced features and comprehensive support, you may consider purchasing the licensed version.
In conclusion, BenchVue Basic offers a fantastic entry point into the world of instrument control and data analysis. It simplifies your workflow and empowers you to achieve your goals efficiently. Download BenchVue Basic and experience the capabilities of BenchVue software, and when you're ready for advanced features and premium support, consider the licensed BenchVue app. It's a journey of continuous improvement and innovation in your field.