A close-up photograph of a digital financial display showing various monetary values in dollars with colored arrows indicating changes.

Test Lab Modernization Trends for Financial Enterprises

Financial enterprises face pressure to test more complex systems, faster than ever, while facing multiple regulatory compliance requirements that must be fulfilled multiple times per year. For many, their current state of testing simply can’t keep up. To address these challenges, a test lab modernization and automation strategy is key to meeting objectives and requirements in the financial sector.

In widespread discussions with financial enterprises about their test labs, several recurring challenges consistently emerge. Many organizations manage multiple labs or environments that are segmented by technology or vendor, often resulting in silos across both customer premises and vendor facilities. These fragmented setups hinder collaboration and scalability. Testing services are commonly sourced from vendors through annual contracts for a pool of resources, often delivered on a best-effort basis with limited guarantees of performance or timeliness.

In addition, typical lab setup times can stretch into weeks, requiring the coordination of multiple lab technicians. In some cases, labs are intentionally kept static to reduce setup time, but this approach significantly limits flexibility and adaptability. Testing cycles themselves are long, running several months with manual report generation, and critically, there is no integration testing performed across environments. This leads to issues surfacing in production environments that were not tested due to the siloed nature of lab operations — significantly increasing incident risk and costs. Furthermore, impairment testing is minimal, and never conducted in an integrated fashion. The result is lengthy timelines for new feature testing — often taking 9 to 12 months to fully develop test plans and execute testing — while redundancies and duplication persist due to overlapping tools and processes across disparate labs.

Regulatory compliance requirements for financial enterprises

Financial enterprises are being continually pushed to test more complex systems, faster than ever before, while trying to reduce costs and carbon footprint. On top of that, they all face multiple regulatory compliance requirements, many that must be fulfilled multiple times per year. For many, their current state of testing simply can’t keep up. Their unique requirements include:

Timely compliance

Consumer duty

Data integrity

Security assurance

Drivers for lab and test modernization in financial enterprises

Objectives voiced by a wide range of financial enterprises include the incorporation of automated Infrastructure as Code (IaC) along with these requirements:

Prime objectives of test lab modernization

To address the drivers above, and to achieve optimal productivity in testing, a  test lab modernization solution for financial enterprises  should abstract physical, virtual, and hybrid lab resources (that may be geographically dispersed) with systems and processes to provide a “federated lab” with access for each test team. Through their solution interface, each test team should be able to reserve lab resources, build templates to define required test topologies, and trigger the fully automated build of any test topology. Teams should have their own lab in a designated timeslot, which can be rapidly reconfigured at will.

Comparison diagram showing serial current-state test lab workflow versus parallel future-state workflow with automated setup, execution, reporting, and analytics.
Sample Current State Test Lab (top) and Future State (bottom)

The interface should also provide a centralized development environment. This allows test teams to build automated test suites, and the controls to execute them, with results populated into a centralized reporting engine that tracks testing progress against their plan. Diverse global test teams from different organizations should possess a comprehensive platform to automate the testing in their continuous integration / continuous delivery (CI/CD)process that is fully compatible with in-house or third-party automation tools.

Learn how Keysight Network Testing for Financial Services solutions can help financial enterprises realize their testing objectives and requirements in the financial sector.

limit
3