Testing HEMS for Grid Modernization
For most of us, energy management at home seems simple. We plug in our devices, turn on the air conditioner, charge the car, and expect the lights to stay on. But behind that everyday convenience, the home is changing quickly.
More homes are adding electric vehicles, rooftop solar panels, battery storage, smart appliances, and connected loads. That means the home is no longer just a place where energy is consumed. It is becoming a more active, intelligent part of the grid.
This is where home energy management systems, or HEMS, come in.
A HEMS helps coordinate how energy flows between the grid, solar panels, battery storage, electric vehicles, EV chargers, and home loads. In practical terms, it can help keep a home operating when the grid is offline, store excess solar energy, make better use of an EV battery through vehicle-to-home or vehicle-to-grid technologies, and respond to time-of-use energy rates.
That sounds promising. But from an engineering perspective, it also introduces a major challenge: how do you know all these systems will work together reliably before they are deployed in a real home, connected to a real grid? That is the focus of our upcoming webinar with James Arnold, Keysight’s high-power and grid test expert. James will explain why HEMS is becoming an important piece of grid modernization.
Register for the webinar. Pick a track that’s convenient for you:
Europe: Wed, July 1
Americas: Thu July 9
Asia Pacific: Wed, July 15
Ensuring Interconnectivity and Interoperability
The grid is moving from a model built primarily around centralized generation to one that must accommodate more distributed energy resources, or DERs, at the edge. Solar inverters, battery energy storage systems, bidirectional EV chargers, and HEMS can all play a role in helping balance supply and demand. But they also need to interoperate across power, communications, controls, cybersecurity, and standards requirements.
The challenge is that HEMS is not a single-device problem. It is a system-level problem. That is why design, emulation, and test need to come together earlier in the development process. For organizations solving complex energy and grid challenges, the ability to recreate real-world conditions in the lab can make the difference between discovering issues late in the field and validating behavior with confidence before deployment.
A realistic HEMS testbed needs to recreate the conditions a home energy system will actually experience. That may include a grid emulator, home load emulation, EV and EVSE emulation, solar PV emulation, battery storage emulation, and automation software to tie everything together. It also needs to support a mix of real and emulated devices, because engineering teams often need flexibility as designs evolve.
This matters because the difficult scenarios are often the most important ones to test. What happens when a large HVAC load kicks on at the same time cloud cover reduces solar output? Can the HEMS detect the change, draw from storage, coordinate the inverter, and maintain stable operation? How does the system behave during voltage sags, outages, frequency shifts, poor power quality, or changing grid signals?
These are not just corner cases. They are the kinds of real-world events that determine whether a HEMS can support resilience, interoperability, and grid modernization in practice.
Standards also add another layer of complexity. In North America, DER interconnection and inverter certification requirements are shaped by standards such as IEEE 1547.1-2020 and UL 1741 SB. In Europe, requirements such as EN 50549 and country-specific grid codes come into play. For EV and EVSE integration, support for modern charging standards, bidirectional charging, and connector types such as CCS and NACS becomes important as companies design for multiple markets.
The good news is that realistic emulation can help engineering teams validate earlier, replicate testing more consistently, and reduce risk before field deployment. By connecting design, emulation, and test, Keysight helps customers move faster, reduce risk, and innovate with greater confidence as they bring new grid-edge technologies to market.
Grid modernization is often discussed at the utility or infrastructure level. But increasingly, part of that modernization is happening inside the home. As HEMS becomes more central to how distributed energy resources are coordinated, engineering teams need mission-critical design enablement that helps them test not only individual components, but the full system behavior that determines real-world performance.
Join me and James Arnold for the upcoming webinar as we explore how HEMS testing is evolving, why realistic testbeds matter, and how engineering teams can build confidence as homes become smarter, more connected, and more grid-interactive.
Contact us for expert advice on grid modernization.