Powering the New Era of Software-Defined Vehicles with Keysight at ATE 2024
The automotive industry is rapidly evolving, marked by advancements in software complexity, vehicle-to-everything (V2X) communication, and electric vehicle (EV) technologies. By 2030, an estimated 4.2 million cars will be autonomous, and over 60% of all cars sold globally will be electric. To spearhead innovations in software-defined vehicles (SDVs), companies need a partner that offers innovative, secure, and comprehensive testing solutions.
This June, join Keysight at the Automotive Testing Expo Europe 2024 (ATE) in Stuttgart as our technical experts showcase the latest design, emulation, and testing solutions to accelerate software-defined vehicle innovations.
Key Innovations to watch at ATE 2024
Accelerate EV charging infrastructure deployment
Discover our Scienlab Charging Discovery System (CDS), a modular and upgradeable solution for testing charging interfaces during high-power charging — up to 1,500 V DC and ±600 A DC. It can emulate charging communication and conduct tests on electrical parameters to ensure conformance and interoperability compliance. With its automated testing capabilities and pre-programmed test cases, this innovative solution enables faster and more efficient deployment of EV charging infrastructures.
Streamline mmWave radar testing
Radars based on a frequency modulated continuous waveform (FMCW) are integral to SDV applications, which operate in the frequency ranges of 24 GHz, 77 GHz, and 79 GHz. Automotive engineers face various testing challenges, including complex test setups, the need for ultra-wideband mmWave measurements, signal-to-noise (SNR) loss, and compliance with evolving industry standards.
To overcome these challenges, we will demonstrate Keysight’s automotive radar transmission (Tx), reception (Rx), and interference testing solutions and how they accelerate the robust analysis of automotive radar signals across full frequency ranges.
Understand FMCW automotive radars
Test vehicle-to-everything (V2X) comprehensively
Comprehensive testing from labs to the field is paramount to ensuring robust vehicle-to-everything (V2X) communications. Keysight’s V2X testing solutions simulate complex V2X test models, perform hardware-in-the-loop and road tests, and evaluate models rigorously in the field. Additionally, our WaveBee toolchain, with the UXM-5G platform, can help streamline V2X integration and testing processes and speed up compliance and interoperability validation across an intelligent transport system (ITS) environment.
Test in-vehicle network (IVN), memory, and SerDes
Whether you aim to verify OSI layers 1–7, ensure OVN signal integrity, or fortify network security, our robust in-vehicle network test solutions have you covered.
At ATE, Keysight experts will demonstrate our full-suite IVN solutions to test waveform, linearity, and jitter for high-speed transmit compliance of 10GBASE-T1. Our demonstrations will feature advanced oscilloscopes like MXR for low bandwidth and UXR for high bandwidth measurements and network-attached storage protocol solutions (NAS) for enhanced security, timing, and network integrity.
Enhance automotive cybersecurity
Keysight’s comprehensive automotive cybersecurity solution covers from the hardware level through all layers of the open systems interconnection (OSI) stack for in-vehicle interfaces, including Wi-Fi, cellular, Bluetooth, CAN, and automotive Ethernet to validate the robustness of electronic control unit (ECU) and telematic control unit (TCU) subcomponents or the entire vehicle.
Check out our latest partnership with ETAS
All these technologies and more will be displayed at Booth 1108, Hall 9. If you cannot attend ATE this year, you may contact the Keysight team to request a personalized demo.
Technical seminars with Microwave Vision Group (MVG)
Keysight and MVG are pleased to host our exclusive seminar and cocktail reception at ATE on June 4. This is a unique opportunity to connect with industry experts and gain insights into the latest automotive testing technologies.
Session 1: Latest Advancements in Antenna and Vehicle Testing
MVG’s Francesco Scotto Di Clemente will provide a comprehensive overview of antenna testing for ground vehicles. The session covers the evolution of antenna testing requirements, technological advancements in GPS, V2V communications, and cellular connectivity, and current regulatory and performance standards. It concludes with insights on future requirements influenced by emerging technologies like 5G, autonomous vehicles, and cybersecurity measures. Save your seat
Session 2: Over-the-Air Antenna Performance Measurements in NTN
Keysight’s Solution Architect Jule Dlugosch will delve into the pivotal role of Over-the-Air (OTA) antenna performance measurements in Non-Terrestrial Networks (NTN). He will also address new challenges, such as lengthy delays and Doppler effects, and explore the complex integration of satellite communications into vehicles. Save your seat
Technical presentations by Keysight
Accurately testing 4D imaging radars with CATR technology
Delve into compact antenna test range (CATR) technology and its impact on 4D imaging radar development. You will also gain practical insights into the CATR technology with real measurement results and its comparison with the traditional approach.
- Speaker: Hock-Yew Yeap
- Time: 12:20 PM, June 5
- Location: Hall 8
In-vehicle network (IVN) security
Discover practical approaches for testing and measuring security components' efficiency and performance for IVN applications. This section will cover topics such as L2 encryption – MACsec, interoperability validation, performance measurements, negative testing and robustness, gateway testing and more. Hear our customers’ case studies on the benefits of system testing versus individual "in-isolation" testing of components.
- Speaker: Ionel Ghita
- Date: 3 PM, June 5
- Location: Hall 10
Meet Keysight at ATE 2024
Do not miss this opportunity to engage with the latest automotive testing technologies and network with industry experts. We are excited to meet you at Booth 1108 at the ATE 2024 Europe.