Achieving C-V2X Compliance
The global connected vehicle market generated $54 billion in 2020 despite the Covid-19 pandemic. Automotive industry predictions indicate this figure will increase to $166 billion by 2025 1. Automotive manufacturers, innovators of intelligent transportation system (ITS) devices, and those responsible for deploying infrastructures must work collaboratively with certified testing specialists. Communication sharing across all industries ensures the technologies brought to market offer interoperability and meet the evolving standards of 5G and C-V2X.
C-V2X certification is a shifting landscape because of the evolving regional ITS standards while at the same time the regulatory requirements for 5G are a moving target. Manufacturers must accommodate future iterations and legislative changes to be competitive in a rapidly expanding marketplace.