Accelerate Time-to-Market of your DER: The Role of Automation in Anti-Islanding Test
Megatrend in the Modern Grid: Energy Demand Is Increasing!
Rapid growth in EV charging infrastructure, AI-driven data centers, and crypto transactions is driving unprecedented energy demand and putting local grid distribution networks under severe stress.
- EV charging: Public charging points grew by 33% in 2024, surpassing 5 million worldwide. Fast and ultra-fast chargers (50% of total) draw significant energy, straining grids in regions like California, Germany, the UK, China, and Norway.
- AI and data centers: AI-powered search and computing consume up to 13x more energy than traditional search, contributing to a 4% rise in U.S. data center energy use in 2024.
- Crypto: Bitcoin alone consumed 130–150 TWh of electricity in 2024—about 0.5% of global electricity use.
In short: Energy demand is rising fast, and the grid is under pressure.
To meet this growing demand, the grid and energy industry is increasingly deploying Distributed Energy Resources (DERs) such as solar plants, battery energy storage systems (BESS), and EVs. While DERs are smaller, faster to deploy, and less expensive than traditional power plants, they also introduce new challenges—from low energy output and security risks to inconsistent standards.
This is where grid compliance testing plays a critical role: ensuring that every DER connected to the grid operates safely, reliably, and in harmony with existing infrastructure.
The Role of Grid Compliance Testing
To overcome these challenges and to ensure that any DER—whether a solar inverter, EV charger, wind turbine, or BESS—can safely and reliably operate when connected to the grid, we use grid compliance testing. These tests are standardized and documented under IEEE 1547.1-2020 and UL 1741 SB. IEEE 1547.1-2020 covers test procedures. UL 1741 SB covers product certification standards and is used by manufacturers to get certified.
IEEE 1547.1-2020 defines various test categories: interconnection and isolation, response to abnormal conditions, active power control, reactive power capability, unintentional islanding, reconnection and synchronization, and many more.
In this blog, we’ll focus on the toughest, meanest, and nastiest test category: Unintentional Islanding or Anti-Islanding Test.
What is the Anti-Islanding Test?
To understand this, we must first understand unintentional islanding. DERs do not operate independently. For a DER to operate, it must synchronize with the grid. It must match the phase, voltage, and frequency of the grid. Once synchronization is complete, the DER keeps running and feeding power to the grid and/or to the local load.
Like every other piece of equipment, DERs require periodic maintenance, so we must disconnect them from the grid. Other reasons—such as grid outages or faults—can also cause breakers to open and disconnect DERs. Traditional power plants, designed to feed power to the grid, stop generating power when disconnected from the grid. However, DERs keep operating and feeding power to local loads even after disconnection. In other words, DERs create unintentional “local islands” with the local loads and continue operating within those islands.
Is this a problem?
Yes, it is a major problem.
- During periodic maintenance, the maintenance engineer opens the circuit breaker and starts maintenance, thinking the island is de-energized. However, the DER is still feeding power.
- If the DER gets disconnected due to a grid outage, it will automatically attempt synchronization when the grid is restored. But the DER is actually feeding power during the synchronization stage. This unsynchronized active power can cause large transients, which can damage the DER and connected loads.
We must absolutely avoid unintentional islanding at all costs. All DERs must have anti-islanding protection, which monitors and detects abnormal grid conditions and disconnects rapidly. As per the IEEE 1547.1-2020 standard, a DER must disconnect within 2 seconds. Every DER must pass the anti-islanding test before it can connect to the grid.
Why is the Anti-Islanding Test so challenging?
The Anti-Islanding Test is difficult because it is extremely challenging and time-consuming to create ideal test conditions in a lab environment.
The biggest challenge is setting up the RLC (Resistor, Inductor, Capacitor) network needed to create a sustained island. Test engineers must finely tune this RLC network to balance real and reactive power for multiple scenarios during the test. Traditional test methods use a physical RLC load bank, where resistors (R), inductors (L), and capacitors (C) are manually adjusted or switched in and out to achieve optimal balancing. This method is not only time-consuming but also requires large, expensive, and fixed RLC load banks.
A traditional anti-islanding test facility requires:
- Large floor space: Typically four to five rooms filled with RLC loads and test equipment.
- Extensive wiring and infrastructure: Engineers must interconnect all equipment manually.
- Environmental control: Air conditioning is required to maintain lab temperature and cool the space.
- Complex software: Separate software is required to control data acquisition.
- 100% manual trial-and-error process: Engineers must repeatedly adjust equipment settings to achieve the required test conditions.
On average, it takes three test engineers more than two weeks to complete a single anti-islanding test!
How Keysight SL1200A Series Simplifies Anti-Islanding Testing
The SL1200A Series Regenerative 3Phase AC Emulator and RP7900 Regenerative Power Supply eliminate almost all of the equipment and resources required by traditional anti-islanding test setups:
- No need for large RLC load banks: The built-in power hardware-in-the-loop (PHIL) technology and RLC auto-tuning algorithm dynamically switch from grid emulator mode to RLC mode, removing the need for dedicated RLC loads.
- No separate data acquisition system required: The integrated measurement system in the SL1200A Grid Emulator and RP7900 DC Source eliminates the need for external data acquisition instruments.
- Minimal infrastructure: All the extensive wiring, interconnections, and environmental controls are significantly reduced.
- Fully automated: The SL1221A Anti-Islanding Conformance Test Automation Software eliminates the 100% manual, trial-and-error process of traditional setups.
- Massive time savings: What used to take three engineers more than two weeks now takes approximately four hours.
A Smarter, Faster Path to Grid Compliance
As the grid evolves and energy demand continues to rise, faster, more reliable grid compliance testing is essential for safely deploying DERs at scale. Traditional anti-islanding test methods simply cannot keep up with the pace of the modern energy transition.
The Keysight SL1200A Series enables manufacturers and test labs to dramatically reduce test time, space, and cost—while improving accuracy and repeatability. By simplifying one of the most challenging grid compliance tests, it helps accelerate innovation, reduce risk, and ensure a safer, more resilient energy future.