A city with lights and text AI-generated content may be incorrect.

Innovating for 6G

As the world eagerly anticipates the arrival of applicable 6G innovations, researchers face numerous challenges in validating this next-generation wireless communication technology. The journey from theoretical concepts and mathematical equations to real-world 6G implementation is complex and requires meticulous planning, testing, and measurements to better characterize these ultra-high frequencies.

Not only must 6G research help uncover specific channel behaviors ─ it also validates how these new frequencies, waveforms, and other capabilities will perform from the physical layer up to the higher-layer protocols. Let’s dive into the challenges that researchers must resolve:

Channel-Level 6G Challenges

Network-Level 6G Challenges

From 6G Theory to Simulation, and Emulation

6G researchers are modeling systems, channel propagation, and waveforms with design simulation software tools.

The next step in this 6G development process is to take these simulations into real-world signal emulation. Emulation is crucial for testing the performance of 6G systems in real-time channels and networks, from the physical layer to higher layer protocols.

Emulating 6G signals in a controlled lab environment enables researchers to accurately assess the performance of 6G systems. This includes evaluating the challenges mentioned earlier under repeatable conditions to fine-tune program iterations against varying scenarios. Researchers can also study system vulnerabilities by emulating cybersecurity issues and addressing them early on.

6G: From Innovative Research to Reality

The industry expects 6G commercialization to happen by 2030 – leaving at best five years to bring to fruition both products and applications which must meet conformance standards that are still in various stages of formulation. Researchers, device and component designers, test and measurement specialists, network and cybersecurity engineers, and regulatory authorities are collaborating across the 6G ecosystem to bring 6G to life.

A building with many windows AI-generated content may be incorrect.

Recently, Keysight had the opportunity to visit the 6G research labs at Northeastern University, where the researchers shared their exciting projects. These covered:

  1. Studying a 130 GHz broadband MIMO system to increase data throughput and transmission distance. The MIMO system uses two data streams with 10 GHz of bandwidth at 130 GHz to achieve a 36 Gbps over-the-air transmission.
  2. Emulating a person-in-the-middle attack scenario to eavesdrop on a highly directional sub-THz communication link. The person-in-the-middle attack scenario uses a metasurface to bend a highly directional sub-THz beam towards an eavesdropper receiver while maintaining the line-of-sight link.
  3. Researching real-time sub-THz for network applications. The real-time sub-THz test bed uses an FPGA prototyping system with high-speed digital-to-analog converters (DACs) and analog-to-digital converters (ADCs), capable of supporting 8-10 GHz of contiguous bandwidth at sub-THz frequencies to get up to 60 Gbps.

Keysight’s production crew captured highlights of these exciting 6G projects, so that we can share them with you in this online event: Innovating for 6G with Keysight & Northeastern University. Pick a date and time that is convenient for you to attend.

Register today!

limit
3