Unlocking the Potential of 6G FR3

6G aims to connect the physical, digital, and human worlds through emerging technology focusing on new spectrum utilization, artificial intelligence (AI) integration into networks and devices, digital twins, and new network architectures. These elements enhance network programmability and automation across various 6G use cases.

While the commercial deployment of 6G seems quite far away, the research needs for 6G are already here, including growing efforts around the spectrum. New frequency ranges are needed to satisfy the bandwidth needs of the ever-growing throughput requirements. Frequency range 3, or FR3, is one of the new spectrum ranges where 6G is evolving. There were only two frequency ranges for 5G: FR1 and FR2. FR3 is between FR1, often referred to as sub-6 GHz, and FR2, the so-called millimeter-wave range, between 7 and 24 GHz.

6G Requirements: A Drive Towards Deterministic Channel Models

4G and 5G addressed radio channel modeling requirements using geometry-based stochastic channel models (GSCMs) for simulating and testing massive multiple-input and multiple-output (mMIMO) systems. However, 6G use cases and technologies are generating new requirements for radio channel modeling because of:

6G FR3 Radio Channel Modeling

Antenna arrays with substantial apertures are under investigation in the 6G FR3 band for MIMO technologies, including MIMO, mMIMO, and xMIMO. xMIMO antenna arrays support narrow pencil beams and more MIMO layers than conventional mMIMO. Figure 1 shows an example of extreme hybrid beamforming, FR3 upper mid-band base station. As a result, the design and validation of xMIMO wireless systems necessitate accurate intra- and inter-cluster angular characteristics from the channel model.

A diagram of a smart phone Description automatically generated

Figure 1. An example of extreme hybrid beamforming, FR3 upper mid-band base station

Ensuring that the channel model accurately captures the intra- and inter-cluster angular characteristics is essential when conducting system simulations or testing the actual performance of xMIMO base stations in RAN and Open RAN configurations. In addition, dynamic channel models are necessary for evaluating beam management and precoding adaptation over user equipment movement. These channel models consider transitions between line-of-sight (LOS) / non-line-of-sight (NLOS) and blockage conditions.

However, the current 3GPP GSCM channel models lack the accuracy needed to develop extreme beamforming algorithms with highly directive pencil beams. To address that, a new 3GPP RP-234018 Release 19 technical study item on channel modeling enhancements for 7 to 24 GHz for New Radio (NR) was initiated.

To test the upper mid-band for FR3, test engineers need:

6G FR3 System Testing

6G FR3 system testing requires phase and time-coherent multichannel emulation using semi-deterministic and deterministic channel models. From the physical layer (PHY) to the application layer, key performance metrics for 6G FR3 testing include:

A close-up of a map Description automatically generated

Figure 2. The three main channel modeling approaches necessary in 5G-Advanced and 6G system simulations, design, and product development and testing.

With a robust channel emulation solution, test engineers can reproduce a diverse propagation environment and emulate hardware impairments like phase noise and interference. They will need:

The Keysight 6G FR3 system test solution

The Keysight 6G FR3 system test solution includes a channel emulator, channel emulation software, and an MXG signal generator. This solution creates realistic and highly accurate stochastic and deterministic models for mimicking 6G FR3 components and systems. The MXG signal generator provides the signal input to the FR3-capable channel emulator. The channel emulator also supports ISAC for detecting and tracking objects.

A computer monitor and electronic equipment Description automatically generated

Figure 3. The Keysight 6G FR3 system test solution

The Bottom Line

Precise channel emulation is crucial for 6G FR3. Accurate channel models are needed to support advanced 6G features and allow for realistic testing of 6G technologies, such as mMIMO and beamforming, under various conditions to understand how these technologies will perform in real-world scenarios. Additionally, it supports advanced use cases like ISAC, which require detailed knowledge of the channel characteristics to function effectively.

Be prepared for 6G and the challenges it brings onboard and accelerate your 6G prototyping before releasing standards using Keysight solutions for channel modeling and emulation for FR3 MIMO, mMIMO, xMIMO, and ISAC.

Contact us for insights and advice on unlocking the frequency bands targeted by 6G and validating new spectral efficiency technologies.

How to Perform 6G FR3 System Test

limit
3