Exploring Antenna Innovation with Keysight at EuCAP 2025

Have you ever wondered how your smartphone, Wi-Fi, or even your car's GPS works so seamlessly? The secret lies in the incredible world of antennas. These unsung heroes of wireless communication are everywhere, making our lives easier and more connected.

A few weeks ago, the 2025 edition of EuCAP (European Conference on Antennas and Propagation) was held in the vibrant city of Stockholm, Sweden. If you’re not familiar with this conference, let me fill you in. EuCAP is the largest antennas and propagation conference in Europe, attracting over 1700 participants from academia and industry. This year's conference showcased the latest technological and scientific discoveries in antennas and propagation, focusing strongly on 5G / 6G, radar, and non-terrestrial network (NTN) technologies. And guess what? The team and I were right there amid it all, soaking up the knowledge and connecting with fellow enthusiasts.

Inspired by the amazing insights from EuCAP, I decided to write about antennas today. Let’s explore how they work, why they are important, how to measure them, and the latest developments in this field. Ready? Let's go!

The Heartbeat of Wireless Communication

Alright, let's get to the heart of the matter—antennas! These nifty devices are like the heartbeat of wireless communication, converting electrical signals into electromagnetic waves and vice versa. It's a bridge between the electrical world (like your phone or radio) and the radio wave world (like signals flying through the air).

They come in all shapes and sizes, each designed for specific tasks. Imagine them as the magic wands that make your devices communicate with each other.

Let’s break down a few types of antennas you’re likely to encounter:

But designing a great antenna is just part of the story. To make sure they perform at their best, we need to measure them precisely. Understanding an antenna’s characteristics is key to building strong, efficient communication systems. Here’s a quick tour through some of the important performance metrics:

So the next time you stream a video, send a message, or scroll through social media—just remember, there’s an entire world of clever antenna engineering making it all possible, one signal at a time. And that world involves some cool testing techniques:

No alternative text description for this image

Figure 1. The Keysight PNA-X Pro VNA in action

Innovations in Antenna Technology

The world of antennas is moving fast—and it's not just about better bars on your phone anymore. With the rapid evolution of wireless tech, antennas are becoming smarter, more precise, and more powerful than ever before.

Here are just a few of the exciting breakthroughs shaping the future:

Beamforming: Techniques that direct signals towards specific users, improving efficiency and reducing interference. Essential for 5G, Wi-Fi 6/7, and radar systems.

Multiple Input Multiple Output (MIMO): Systems that use multiple antennas to enhance data throughput and reliability. It's at the heart of everything from smartphones and routers to satellite communication systems.

5G Antennas: Designed specifically for ultra-fast, low-latency connections, these antennas are paving the way for real-time experiences like remote surgery, self-driving cars, and immersive augmented reality (AR) / virtual reality (VR).

Evolving Use Cases

The innovation doesn’t stop there. Antennas are also expanding into non-terrestrial and next-gen communication systems:

Keysight at EuCAP 2025

Figure 2. Keysight experts engaging with attendees at EuCAP 2025

Now, let’s zoom in on EuCAP 2025, where the antenna world came together—and where Keysight was front and center. EuCAP 2025 introduced exciting new themes, including:

We’ve Got You Covered: Keysight’s Antenna Testing Solutions

When it comes to pushing antenna tech forward, it’s not just about theory—it’s about precision measurement. That’s where Keysight shines. Here are some of the top tools engineers are using / can use to turn ideas into real-world performance:

S7601A Antenna Measurement Toolset: Designed to test and verify different types of antennas for cellular, automotive, and satellite communication. Key features include spherical antenna pattern measurements, phased array control and calibration, and a GUI for manipulating patterns in 2D, 3D, and tabular formats.

A machine with a computer and monitor AI-generated content may be incorrect.

Figure 3. The Keysight Antenna Measurement Toolset

F9650A Compact Antenna Test Range (CATR): Offers quiet zone diameters of 30 and 40 cm, operating from 6-110 GHz. This modular format is ideal for precise antenna testing in a controlled environment.

FieldFox Handheld Analyzers: Perfect for field measurements, these portable devices offer features like CalReady and QuickCal for easy calibration, making them ideal for on-site testing and troubleshooting.

A close-up of a gps device AI-generated content may be incorrect.

Figure 4. The Keysight 85574A Handheld Direction Finding Antenna with the Keysight FieldFox

Vector Network Analyzers (VNAs): Measure how antennas behave across different frequencies, providing insights into S-parameters, gain, efficiency, and more to ensure optimal antenna performance.

Anechoic Chambers: For precise measurement of radiation patterns and gain, Keysight offers full-sized anechoic chambers. These chambers eliminate external noise, allowing for accurate and reliable antenna measurements.

The Bottom Line

Antennas are the backbone of our connected world. Understanding their principles, measurement techniques, and innovations is key to optimizing performance and ensuring seamless connectivity. As technology continues to advance, antennas will play an even more critical role, paving the way for a future where everything is connected. So next time you use your smartphone or Wi-Fi, take a moment to appreciate the magic of antennas working behind the scenes.

Keysight provides a range of top-notch solutions for antenna testing, ensuring your antennas perform at their best. Whether you're testing in the field or measuring with VNAs, Keysight has you covered. So next time you're working on antenna testing, remember the reliable solutions from Keysight.

Want to meet us? Check out the list of our upcoming events and join us for more insightful sessions and demos!

eBook: Antenna Performance Tips

Learn Hub: Phased Array Antenna Design and Test

Use Case: How to Test Phased Array Antennas

eBook: How to Design and Test a Phased Array Antenna

limit
3