Patrick Le Houillier
Senior Application Engineer
Born in Ottawa, Canada in 1975, Patrick graduated from École Polytechnique de Montréal in 1999 in the Engineering for Physics program, specializing in photonics and micro-electronics engineering. His expertise involves advanced fiber coupling and medical illumination device design. After 5 years in the hardware components industry, Patrick moved to the United States, first at Lambda Research Inc. in 2005, working with TracePro, and joined Optical Research Associates two years later to work with LightTools as an Illumination Solutions Engineer. Patrick is now the senior LightTools Application Engineer in North America and focuses on pre-sales support, examples developement as well as Measurement devices and services support.