testcase TC_MS_GHF_HO_INI_MS_BV_H001() runs on ServerSyncComp system TwinTestAdapter {...}
Generated with T3Doc 2.0 on Fri Sep 05 17:01:28 CEST 2008.

Description

Test Strategy:
- The IUT is operating with BS1(served BS).
- DCD is set to send a trigger TLV that requires the IUT to send MOB_MSHO-REQ,
when the Serving BS metric is less than the Trigger value.
- BS2(Target BS)is activated.
- The IUT proceed with Cell reselection with BS2(Target BS)by scanning,optionally
with association,BS2(target BS).
- Serving BS(BS1)metric decreased under the metric value,this triggers the HO decision for the IUT(MS)
- The IUT sends a MOB_MSHO_REQ message to BS1.
- The tester sends a MOB_BSHO-RSP message with HO operation mode = "0b1" to the IUT
- The IUT sends a MOB_HO-IND message with HO_IND_type = "0b00"


Purpose

Initial Conditions:
IUT has completed initial network entry and is operating.
IUT has transmitted its first MOB_MSHO-REQ message.
Target BS is available.

Test Purpose:
Check that: having received a valid MOB_BSHO-RSP message with HO operation mode = "0b1"
and the IUT can treat the HO request as accepted,
sends a MOB_HO-IND message with HO_IND_type = "0b00".