Microsoft Internet Explorer Internet Messaging API Information Disclosure

Strike ID:
E16-5jm01
CVSS:
5.3 CVSS:3.0/AV:N/AC:H/PR:N/UI:R/S:U/C:H/I:N/A:N
False Positive:
f
Variants:
144
Year:
2016

Description

This strike exploits an information disclosure vulnerability in Microsoft Internet Explorer. Specifically, when the loadXML function is called on an MSXML DOMDocument with URI set to a malicious MHTML URI, it is possible to discern whether or not a file exists on the target system through errors that are reported back to the user of whether or not that file exists. A malicious user can use abuse this funcitonality to disclose this information about the target user's system.

CVE

Bid