Datenblätter
Introduction
The Keysight Technologies, Inc. N5435A Infiniium server-based license allows you to move your oscilloscope application license from one Infiniium oscilloscope to another, using a license server. Just check out the license from the server when you need it, and return it when you are finished with it. You can check out the license in increments of days. If you forget to return the licenses, the oscilloscope will automatically return them for you when the allotted time expires.
License files for the N5435A Infiniium server-based license are supported across Infiniium Series oscilloscope platforms, as well as the N8900A Infiniium Offline oscilloscope analysis software, so you can protect your application software investment.
Infiniium Application Server License: How It Works
The N5435A Infiniium server-based license is ideal for companies with multiple Infiniium oscilloscopes. You can share license files across oscilloscopes, anywhere in the world.
To borrow licenses, the oscilloscope needs to be connected to a LAN to access the license server. Once you obtain the necessary licenses, you do not need to remain connected to the LAN. Just reconnect when you decide to return your borrowed licenses to the license server. If you forget to return the license within your borrowing period (in units of days), that is not a problem. Both the license server and the Infiniium oscilloscope have their own time counters tracking the valid period for the license. Once a particular license expires, the license server automatically returns the credit to that specific license file. At the same time, the Infiniium oscilloscope automatically loses the license.
If you already have some node-locked licenses installed on your Infiniium oscilloscope, that is not a problem. The N5435A Infiniium application server license automatically populates the list with available server-based licenses that your oscilloscope does not have.
Which License Type Is Best For You?
There are several different types of Infiniium oscilloscope application software licenses available from Keysight. Choose the type that works best for your situation.
Server-based licenses are generally recommended for companies that want to share licenses across multiple Infiniium oscilloscopes and/or the N8900A Infiniium Offline application.
Node-locked licenses are recommended for teams that want to ensure specific oscilloscopes retain specific licenses indefinitely.
×
*Indicates required field
Thank you.
A sales representative will contact you soon.