testcase TC_BS_ARQ_TXD_BV_H010a() runs on Simu system TestAdapter {...}
Generated with T3Doc 2.0 on Fri Jan 30 15:06:31 CET 2009.

Configuration

Specific requirements:
- REG:
- ARQ supported
- Packing supported
- DL SF:
- ARQ requested
- ARQ window size set to 32
- ARQ block size set to 16
- Packing enabled


Description

Test Strategy:
- Send an Echo Request to receive an Echo Reply
- Send an ARQ feedback IE using the cumulative ACK (type 1)in a stand
alone ARQ feedback management message. It NACKs one of the blocks.
- Check that the IUT(=SS) retransmits the NACKed block.

Note: It is required that the ARQ_BLOCK_LIFETIME >= N x ARQ_RETRY_TIMEOUT where N is
greater than 1.



Purpose

TP/BS/ARQ/TXD/BV-H010a
TP version: 0.0.14
Initial condition: An ARQ connection is established and the IUT is the transmitter on this connection.
The IUT has transmitted ARQ blocks all of which have been acknowledged except one.
Test purpose: Check that: On not receiving an ACK concerning this block using cumulative ACK (type1)
(this block is now in the "Waiting" state), the IUT retransmits the block that was not
ACK?ed.