您希望搜索哪方面的内容?
X 系列信号分析仪 LTE FDD IVI 和 MATLAB 仪器驱动程序
For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers
This driver download installs the IVI-C, IVI-COM, and MATLAB driver components.
Keysight instrument drivers also require that Keysight IO Libraries Suite be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite
Current Version Details | |
---|---|
Version | 1.0.7.0 |
Models Supported | N9010A, N9020A, N9030A |
IO Libraries Required Version | 16.0 or greater |
Driver Types and Version | IVI-C (32-bit/64-bit) IVI-COM (32-bit/64-bit) MATLAB (32-bit/64-bit) |
IVI Classes Supported | IviDriver 1.0 |
Minimum IVI Shared Components Version | 2.2.1.0 |
发布日期 | 版本 | 版本说明 |
---|---|---|
2019-09-26 | 1.1.7.0 | Added M8920A, M90XA, N9041B Model Support. |
发布日期 | 版本 |
---|---|
2019-09-26 | 1.1.7.0 |
版本说明 |
---|
Added M8920A, M90XA, N9041B Model Support. |
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0
IVI Generation: IVI-2014
如何下载
- Click the Download button
- Select the appropriate executable file
- Choose Run
如何安装
Run the downloaded installer
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC / Instrument
操作系统
- Windows 8
- Windows 7
- Windows 10
前提要求
支持的仪器
- N9010A, N9020A, N9030A, N9000B, N9010B, N9020B, N9030B, N9040B, N9041B, N9000A, SPN9026A, SPN9003A, M9290A, M9420A, M9421A, M8920A, M90XA
相关链接
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0
IVI Generation: IVI-2014
如何下载
- Click the Download button
- Select the appropriate executable file
- Choose Run
如何安装
Run the downloaded installer
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC / Instrument
操作系统
- Windows 8
- Windows 7
- Windows 10
前提要求
支持的仪器
- N9000A, N9010A, N9020A, N9030A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A
相关链接
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0
IVI Generation: IVI-2014
如何下载
- Click the Download button
- Select the appropriate executable file
- Choose Run
如何安装
Run the downloaded installer
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC / Instrument
操作系统
- Windows 8
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- N9010A, N9020A, N9030A
相关链接
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0
IVI Generation: IVI-2014
Version Description:
- Updated help file
- Added IVI-2014 Compliance
- Rebranded as Keysight Technologies
- Bug Fix: Previous versions of this driver contained COM GUID's that conflicted with the KeysightSAn IVI driver. If both drivers were installed, the drivers could become unusable. This issue has been fixed by replacing the conflicting COM GUID's in this driver.
如何下载
- Click the Download button
- Select the appropriate executable file
- Choose Run
如何安装
Run the downloaded installer
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC / Instrument
操作系统
- Windows 8
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- N9010A, N9020A, N9030A
相关链接
如何下载
- Click the Download button
- Select the appropriate executable file
- Choose Run
如何安装
Run the downloaded installer
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC / Instrument
操作系统
- Windows 8
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- N9010A, N9020A, N9030A