What are you looking for?
FrameScope /WireScope 350 Download
FrameScope/WireScope 350 Download:
Download the latest software package for your WireScope / FrameScope 350 product - Version 3.2.8 :
NOTE:
You must uninstall the previous version of ScopeData Pro prior to installing the new software. Failing to do so may cause unpredictable behavior.
This Version Includes:
- ScopeData Pro for the PC
- FrameScope 350 for the FrameScope 350/Dual Remote 350
- WireScope 350 for the WireScope/Dual Remote 350
- WireScope 155 v 5.21 for the WireScope/Dual Remote 155 (English version only)
New Features Added
Network Testing
- Frame Loss Rate tests and Back-to-Back tests had been added into the RFC 2544 Testing.
- Inter-operability between FrameScopeTM 350 and FrameScopeTM Pro for RFC 2544 Testing.
- RFC 2544 web report enhancement.
Cable Testing
- Latest updates of cables and connectors databases.
NOTE: After installing software version 3.2.8 or later, the main cabling screen on the WireScope 350 or FrameScope 350 displays a new simplified user interface with Class D and Class E buttons. If you would like to return to the original "Expert Mode" screen, please see the instructions below.
Download the "Software Upgrade Utility Guide" for FrameScope / WireScope 350 (3.2 MB)
Please read chapter 8 for Software Upgrade Utility Guide for FrameScope / WireScope 350.
Release Date | Version | Version Description |
---|---|---|
2003-08-24 | 5.20 | Version 5.20 includes many new major features. |
Release Date | Version |
---|---|
2003-08-24 | 5.20 |
Version Description |
---|
Version 5.20 includes many new major features. |
How to Download
See Above
How to Install
- Information Not Available
Licensing
- Does Not Require a License
Supporting Documentation
How to Download
See Documentation
How to Install
See Documentation
Licensing
- Does Not Require a License
Supporting Documentation
Installs on: PC
Prerequisites
See Documentation
Supported Instruments
- WireScope, FrameScope 350, N2600A, N2610A
Download the latest software package for your WireScope / FrameScope 350 product.
Version 3.0.3 Includes:
ScopeData Pro v 3.0.3 for the PC
- FrameScope 350 v 3.0.3 for the FrameScope 350/Dual Remote 350
- WireScope 350 v 3.0.3 for the WireScope/Dual Remote 350
-
WireScope 155 v 5.21 for the WireScope/Dual Remote 155
Version 3.0.3 major features include:
- Limit Update: TIA Category 6 Final Release
- Software Localized into 6 languages
- Locate Switch Port tool added to tools menu
- Additional protocols to Statistics tool
- Improved web based remote control
NOTE: After installing software version 3.0.1 or later, the main cabling screen on the WireScope 350 or FrameScope 350 displays a new simplified user interface with Class D and Class E buttons. If you would like to return to the original "Export Mode" screen, please see the instructions below.
Quick Start Guide for WireScope / FrameScope 350 Software Version 3.0
This document explains the major user interface differences between 3.0 and 2.1 WireScope / FrameScope 350 Software Versions.
** To view the "Expert Mode" Autotest screen perform the following:
- Press the SYSTEM button,
- Then select USER INTERFACE
- Press EDIT
- Select the check box to enable EXPERT MODE
- Press OKAY
- Finish by pressing the MAIN MENU button.
This will bring you back to the "Expert Mode" Autotest screen.
WireScope Software Upgrades
WireScope 155 Software Version 5.20
Version 5.20 major features include:
- Support for Gigabit Ethernet testing over twisted-pair & fiber
- Support for emerging Category 5E cable and Level IIE tester requirements
- Faster Category 5E Network test times
How to Download
See Documentation
How to Install
See Documentation
Licensing
- Does Not Require a License
Supporting Documentation
Installs on: PC
Prerequisites
See Documentation
Supported Instruments
- WireScope, FrameScope 350, N2600A, N2610A