Read the license agreement before downloading the Uncertainty Calculator program.
To do so, scroll down to Supporting Documentation and click License Agreement. By downloading this Uncertainty Calculator program, you agree to be bound by the terms of this license agreement. If you do not agree to all of these terms, do not download the program.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2023-10-02 A.05.00.023.0000 The Uncertainty Calculator helps you determine measurement uncertainty due to your vector network analyzer and calibration kit. This version supports N7562/64A.
Release Date Version
2023-10-02 A.05.00.023.0000
Version Description
The Uncertainty Calculator helps you determine measurement uncertainty due to your vector network analyzer and calibration kit. This version supports N7562/64A.

How to Download

  • Click the Download button and download to your computer either 32 bit or 64 bit installer. If you have a 32 bit operating system, install the 32 bit version. Otherwise, install the 64 bit version. Note, the 64 bit installer will install the files needed for both the 32 bit and 64 bit office versions in the location where the spreadsheet will look for.

How to Install

  1. After you click the download button, you will have the option to Run or Save. Select Run.
  2. Both the 64 bit and 32 bit installers place Readme.txt, Change Log.txt, and VNAUncert.dll in C:\Program Files\Keysight\VNA Uncertainty. The 64 bit installer also places VNAUncert64.dll in the same directory.
  3. The installer places KeysightUncert.xlsm in C:\Users\Public\Documents\Keysight. This is the spreadsheet to be opened with Excel.
  4. After opening the spreadsheet in Excel, select the [Select Network Analyzer] button.
  5. Follow the instructions provided in the program to display measurement uncertainty data.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 10

Prerequisites

  • Information Not Available
No previous versions available
SHOW MORE