How many traces can be displayed when the 4395A's overlay trace function is used?
The number of traces that can be displayed by using the overlay trace function of the 4395A depends on the number of sweep points (NOP) as shown in the following examples:
Example:
NOP 201: 16 traces
NOP 401: 8 traces
NOP 801: 4 traces