Choose a country or area to see content specific to your location
-
PRODUCTS AND SERVICES
- Oscilloscopes
-
Analyzers
- Spectrum Analyzers (Signal Analyzers)
- Network Analyzers
- Logic Analyzers
- Protocol Analyzers and Exercisers
- Bit Error Ratio Testers
- Noise Figure Analyzers and Noise Sources
- High-Speed Digitizers and Multichannel DAQ Solutions
- AC Power Analyzers
- DC Power Analyzers
- Materials Test Equipment
- Device Current Waveform Analyzers
- Parameter / Device Analyzers and Curve Tracers
- Meters
- Generators, Sources, and Power Supplies
- Software
- Wireless
- Modular Instruments
- Network Test and Security
- Network Visibility
- Services
- Additional Products
- All Products, Software, Services
- Learn
- Buy
- Support
- Home
- Software Details
- Software Details
What are you looking for?
Example Programs for the Keysight N5700 Family of DC Power Supplies
This self-executing zip file contains an example program for the Keysight N5700 DC Power Supplies. To download, click on the link below and either run the program from its current location or save it to a hard drive. Execute the program. The installation directory defaults to C:\Program Files\Keysight\N5700 or the user can specify the directory to install the sample programs.
This file contains an example in the following program languages with the following IO libraries:
- C++ with VISA
- Microsoft Visual C++ 6.0 with VISA
- Microsoft Visual Basic 6.0 with VISA and VISA-COM
- Microsoft Excel with VISA
- Keysight VEE with Direct I/O
The sample program is called EZSample. This is a simple example that sets voltage, current, and the protection features of the N5700 Power Supplies. It also measures voltage. This is a perfect introduction to programming the N5700 DC Power Supplies.
Related Links
- © Keysight Technologies 2000–2024
- Privacy
- Sitemap
- Terms
- Trademark Acknowledgements
- Feedback
- Accessibility