On the ENA 6 series, can I get TTL signal indicating Pass/Fail of the limit test like the 871x?
(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)
Yes. The Handler interface can be used. Note that the definition is different from the 871x. In the E5061A/62A and E5061B, level-high means "Pass" and low means "Fail".