Starting Download..
save Save

If I have five slots with HDMI signal testing at the same time, will I be able to test HDCP Prod Keys on five TV sets ..

Yes, you can test HDCP Prod Keys on five TV sets using the U8101A Display Tester, even if you have five slots with HDMI signal testing at the same time. Press the HDCP button on the U8101A. The display will show the cards that are supported by HDCP (eg. HDMI, DVI). If HDMI/DVI cards are available, you can turn on either a selected card or all of the cards.

Was this helpful?


Didn't find what you're looking for?