How do I remotely transfer screen images from my ESA/PSA Series Spectrum Analyzer using Visual Basic 6?
Disclaimer:
You have a royalty-free right to use, modify, reproduce and distribute the Sample Application Files (and/or any modified version) in any way you find useful, provided that you agree that Keysight Technologies has no warranty, obligations or liability for any Sample Application Files.
Keysight Technologies provides programming examples for illustration only, This sample program assumes that you are familiar with the programming language being demonstrated and the tools used to create and debug procedures. Keysight Technologies support engineers can help explain the functionality of Keysight Technologies software components and associated commands, but they will not modify these samples to provide added functionality or construct procedures to meet your specific needs.
Description:
The example program, screen.bas, is written for the PSA and ESA Series Spectrum Analyzers. It transfers the current screen image on the analyzer over GPIB or LAN and stores the image on your PC in the current directory as screen.gif.
screen.exe in the compiled executable of screen.bas.
You can try it out by connecting up a PSA and ESA Series Spectrum Analyzers to GPIB address 18 and running the program. It will store the current screen image as
picture.gif in the directory you run the executable from.
Languages Supported:
Visual Basic 6
Additional Requirements:
None
Revision Date:
August 2003
Download Instructions:
Save the self extracting file to disk. Extract the files and place them in your current Visual Basic 6 working directory.
Procedure:
Set the GPIB address of the instrument to address 18. Connect the GPIB cable and execute program. The screen image will be saved to a file named picture.gif in your working directory.