Can I hide the softkey menu when I perform "Dump Screen Image" on the ENA / ENA-L?
(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)
Yes.
- Press the hardkey of "Entry off (softkey on/off)" in order to hide the softkey.
- Press the hardkey of "system (capture)", so the image without the softkey displayed on the LCD screen is temporarily saved into the internal memory (clipboard).
- Press the softkey of "Dump Screen Image" (system > Dump Screen Image) "to save the screen snapshot in the HDD or FDD".